SLYS053B November 2023 – June 2024 TMAG3001
PRODUCTION DATA
Figure 7-11 shows an example for the omnipolar switch mode where the device is sensitive to either the positive or negative thresholds. The omnipolar switch mode is particularly useful in cases where the magnet polarity is not controlled during the manufacturing process. In this mode, the same thresholds are used for both the polarities. BOP represents the operating point for the switch above which the INT pin switches states. BRP, represents the reverse operating point, below which the INT pin returns to the previous operating state. This mode is similar to unipolar switch mode.