SLYS053B November 2023 – June 2024 TMAG3001
PRODUCTION DATA
The TMAG3001 features an integrated angle calculation so the device can be used as an angle switch for any two axes set by ANGLE_EN. The device is configured as an angle switch, when INT_Mode[2:0] is set to 5h. The THR_Config_1 register acts as A_TH_REF, that sets the reference threshold for the angle crossing. The THR_Config_2 register acts as A_TH_BAND, that determines the threshold region for the angle crossing detection. Figure 7-14 shows the response of the device where the switch output is set to ON state and when the measured angle is above the θTH_REF + θTH_BAND or below θTH_REF + θTH_BAND. The switch output is set to OFF state if the switch output crosses below the hysteresis value set by θANG_HYS. Figure 7-15 shows the response of the device, based on the configured thresholds and hysteresis.