SBAS934A June 2020 – December 2021 TMAG5170-Q1
PRODUCTION DATA
Figure 7-14 shows both regular and special SDO frames during SDI read command. The TMAG5170-Q1 implements in-frame communication. When the controller sends a register read command during a regular read cycle, the corresponding 16-bit register data is sent through the SDO line in the same frame. During the special read cycle, the TMAG5170-Q1 ignores the address and data bits of the SDI line and sends the two channel data set through the SDO line as defined in the DATA_TYPE register bits.