SBAS934A June 2020 – December 2021 TMAG5170-Q1
PRODUCTION DATA
This diagnostic mechanism continuously monitors the internal regulator that supplies the internal digital core, and puts the device in reset if the digital core cannot function reliably. The occurrence of the fault is detected by reading the CFG_RESET bit which can only be set at power up or if the digital core was reset.
Run Mode | Continuous |
Data Sheet Parameters | N/A |
Fault Register Bit | CFG_RESET |
Impact if disabled | N/A. Cannot be disabled. |