SLYS054A March 2024 – April 2024 TMAG5213
PRODUCTION DATA
The TMAG5213 is sensitive to the magnetic field component that is perpendicular to the marked side of the package. This direction is defined as the Z-axis as shown in Figure 7-1. Figure 7-2 shows that a positive magnetic field is defined in this document as what occurs when a south pole is near the marked side of the package. A negative magnetic field occurs when a north pole is near the marked side of the package.