SLOS887F September 2014 – June 2022 TMP112-Q1
PRODUCTION DATA
As an example, if the user is concerned only about the temperature accuracy between –15°C to 50°C, the worst-case accuracy could be determined by using the two slope calculations shown in Equation 2 and Equation 4:
The same calculations must be applied to the minimum case:
Based on these calculations, a user can expect a worst-case accuracy of 0.58°C to –0.5°C in the temperature range of –15°C to 50°C.