SBOS486I July 2009 – December 2018 TMP303
PRODUCTION DATA.
Select the appropriate TMP303 device that matches the application requirements; see the Device Options table for different trip point ranges. Connect the HYSTSET0 and HYSTSET1 pins according to the application requirements; see Table 1. In Figure 13 the TMP303 device is configured with a 1°C hysteresis window (that is, HYSTSET0 = HYSTSET1 = GND). Place a 0.1-µF bypass capacitor close to the TMP303 device to reduce the noise coupled from the power supply.