SPRS841E March 2012 – October 2019 TMS320C6652 , TMS320C6654
PRODUCTION DATA.
Refer to the PDF data sheet for device specific package drawings
The reset controller detects the different type of resets supported on the C6654 and C6652 devices and manages the distribution of those resets throughout the device.
The device has several types of resets:
Table 6-8 explains further the types of reset, the reset initiator, and the effects of each reset on the device. For more information on the effects of each reset on the PLL controllers and their clocks, see Section 5.7.2.
RESET TYPE | INITIATOR | EFFECT ON DEVICE WHEN RESET OCCURS | RESETSTAT
PIN STATUS |
---|---|---|---|
POR
(Power On Reset) |
POR pin active low RESETFULL pin active low |
Total reset of the chip. Everything on the device is reset to its default state in response to this. Activates the POR signal on chip, which is used to reset test/EMU logic. Boot configurations are latched. ROM boot process is initiated. | Toggles RESETSTAT pin |
Hard reset |
RESET pin active low Emulation PLLCTL register (RSCTRL) Watchdog timers |
Resets everything except for test/EMU logic and reset isolation modules. Emulator and reset Isolation modules stay alive during this reset. This reset is also different from POR in that the PLLCTL assumes power and clocks are stable when device reset is asserted. Boot configurations are not latched. ROM boot process is initiated. | Toggles RESETSTAT pin |
Soft reset |
RESET pin active low PLLCTL register (RSCTRL) Watchdog timers |
Software can program these initiators to be hard or soft. Hard reset is the default, but can be programmed to be soft reset. Soft reset will behave like hard reset except that EMIF16 MMRs, DDR3 EMIF MMRs, sticky bits in PCIe MMRs, and external memory contents are retained. Boot configurations are not latched. ROM boot process is initiated. | Toggles RESETSTAT pin |
C66x CorePac local reset |
Software (through LPSC MMR) Watchdog timers LRESET pin |
MMR bit in LPSC controls C66x CorePac local reset. Used by watchdog timers (in the event of a time-out) to reset C66x CorePac. Can also be initiated by LRESET device pin. C66x CorePac memory system and slave DMA port are still alive when C66x CorePac is in local reset. Provides a local reset of the C66x CorePac, without destroying clock alignment or memory contents. Does not initiate ROM boot process. | Does not toggle RESETSTAT pin |