SPRS565D April 2009 – June 2014 TMS320C6743
PRODUCTION DATA.
Refer to the PDF data sheet for device specific package drawings
The device DSP generates the high-frequency internal clocks it requires through an on-chip PLL.
The PLL requires some external filtering components to reduce power supply noise as shown in Figure 6-8.
The input to the PLL is either from the on-chip oscillator or from an external clock on the OSCIN pin. The PLL outputs seven clocks that have programmable divider options. Figure 6-9 illustrates the PLL Topology.
The PLL is disabled by default after a device reset. It must be configured by software according to the allowable operating conditions listed in Table 6-4 before enabling the DSP to run from the PLL by setting PLLEN = 1.
NO | PARAMETER | Default Value | MIN | MAX | UNIT |
---|---|---|---|---|---|
1 | PLLRST: Assertion time during initialization | N/A | 1000 | N/A | ns |
2 | Lock time: The time that the application has to wait for the PLL to acquire locks before setting PLLEN, after changing PREDIV, PLLM, or OSCIN | N/A | N/A | ![]() |
OSCIN cycles |
3 | PREDIV | /1 | /1 | /32 | |
4 | PLL input frequency
( PLLREF) |
12 | 30 (if internal oscillator is used)
50 (if external clock source is used) |
MHz | |
5 | PLL multiplier values (PLLM) (1) | x20 | x4 | x32 | |
6 | PLL output frequency. ( PLLOUT ) | N/A | 300 | 600 | MHz |
7 | POSTDIV | /1 | /1 | /32 |