SPRS945G January 2017 – January 2023 TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1
PRODUCTION DATA
The CPU is a 32-bit fixed-point processor which draws from the best features of digital signal processing; reduced instruction set computing (RISC); and microcontroller architectures, firmware, and tool sets.
The features include:
For more information on CPU architecture and instruction set, see the TMS320C28x CPU and Instruction Set Reference Guide. For more information on the C28x Floating-Point Unit (FPU), see the TMS320C28x Extended Instruction Sets Technical Reference Manual. All of the features of the C28x documented in the TMS320C28x CPU and Instruction Set Reference Guide apply to the C28x+VCU. All features documented in the TMS320C28x Extended Instruction Sets Technical Reference Manual apply to the C28x+FPU+VCU. A brief overview of the FPU, TMU, and VCU-Type 0 is provided here.
An overview of the VCU-I instructions can be found in the TMS320C28x Extended Instruction Sets Technical Reference Manual.