SPRSP25A June 2018 – July 2018 TMS320F28035-EP
PRODUCTION DATA.
To receive notification of documentation updates, navigate to the device product folder on ti.com. In the upper right corner, click on Alert me to register and receive a weekly digest of any product information that has changed. For change details, review the revision history included in any revised document.
The current documentation that describes the processor, related peripherals, and other technical collateral is listed below.
Errata
TMS320F2803x Piccolo™ MCUs Silicon Errata describes known advisories on silicon and provides workarounds.
CPU User's Guides
TMS320C28x CPU and Instruction Set Reference Guide describes the central processing unit (CPU) and the assembly language instructions of the TMS320C28x fixed-point digital signal processors (DSPs). It also describes emulation features available on these DSPs.
Peripheral Guides
TMS320F2803x Piccolo System Control and Interrupts Reference Guide describes the various interrupts and system control features of the 2803x microcontrollers (MCUs).
C2000 Real-Time Control Peripherals Reference Guide describes the peripheral reference guides of the 28x digital signal processors (DSPs).
TMS320x2803x Piccolo Boot ROM Reference Guide describes the purpose and features of the boot loader (factory-programmed boot-loading software) and provides examples of code. It also describes other contents of the device on-chip boot ROM and identifies where all of the information is located within that memory.
TMS320x2802x, 2803x Piccolo Analog-to-Digital Converter (ADC) and Comparator Reference Guide describes how to configure and use the on-chip ADC module, which is a 12-bit pipelined ADC.
TMS320x2802x, 2803x Piccolo Enhanced Pulse Width Modulator (ePWM) Module Reference Guide describes the main areas of the enhanced pulse width modulator that include digital motor control, switch mode power supply control, UPS (uninterruptible power supplies), and other forms of power conversion.
TMS320x2802x, 2803x Piccolo High Resolution Pulse Width Modulator (HRPWM) Reference Guide describes the operation of the high-resolution extension to the pulse width modulator (HRPWM).
TMS320x2802x, 2803x Piccolo Serial Communications Interface (SCI) Reference Guide describes how to use the SCI.
TMS320F2802x, 2803x Piccolo Enhanced Capture (eCAP) Module Reference Guide describes the enhanced capture module. It includes the module description and registers.
TMS320x2802x, 2803x Piccolo Serial Peripheral Interface (SPI) Reference Guide describes the SPI - a high-speed synchronous serial input/output (I/O) port - that allows a serial bit stream of programmed length (1 to 16 bits) to be shifted into and out of the device at a programmed bit-transfer rate.
TMS320x2802x, 2803x Piccolo Inter-Integrated Circuit (I2C) Module Reference Guide describes the features and operation of the inter-integrated circuit (I2C) module.
TMS320x2803x Piccolo Control Law Accelerator (CLA) Reference Guide describes the operation of the Control Law Accelerator (CLA).
TMS320F2803x Piccolo Local Interconnect Network (LIN) Module User's Guide describes the operation of the Local Interconnect Network (LIN) Module.
TMS320x2803x Piccolo Enhanced Quadrature Encoder Pulse (eQEP) Module Reference Guide describes the operation of the Enhanced Quadrature Encoder Pulse (eQEP).
TMS320x2803x Piccolo Enhanced Controller Area Network (eCAN) Reference Guide describes the operation of the Enhanced Controller Area Network (eCAN).
TMS320x2803x Piccolo High Resolution Capture (HRCAP) Reference Guide describes the operation of the High-Resolution Capture (HRCAP) module.
Tools Guides
TMS320C28x Assembly Language Tools v17.9.0.STS User's Guide describes the assembly language tools (assembler and other tools used to develop assembly language code), assembler directives, macros, common object file format, and symbolic debugging directives for the TMS320C28x device.
TMS320C28x Optimizing C/C++ Compiler v17.9.0.STS User's Guide describes the TMS320C28x C/C++ compiler. This compiler accepts ANSI standard C/C++ source code and produces TMS320 DSP assembly language source code for the TMS320C28x device.
TMS320C28x Instruction Set Simulator Technical Overview describes the simulator, available within the Code Composer Studio for TMS320C2000 IDE, that simulates the instruction set of the C28x core.
Application Reports
Semiconductor Packing Methodology describes the packing methodologies employed to prepare semiconductor devices for shipment to end users.
Calculating Useful Lifetimes of Embedded Processors provides a methodology for calculating the useful lifetime of TI embedded processors (EPs) under power when used in electronic systems. It is aimed at general engineers who wish to determine if the reliability of the TI EP meets the end system reliability requirement.
Semiconductor and IC Package Thermal Metrics describes traditional and new thermal metrics and puts their application in perspective with respect to system-level junction temperature estimation.
Oscillator Compensation Guide describes a factory supplied method for compensating the Piccolo internal oscillators for frequency drift caused by temperature.
Piccolo MCU CAN Module Operation Using the On-Chip Zero-Pin Oscillator.
The TMS320C2803x/TMS320F2806x series of microcontrollers have an on-chip zero-pin oscillator that needs no external components. This application report describes how to use the CAN module with this oscillator to operate at the maximum bit rate and bus length without the added cost of an external clock source.
An Introduction to IBIS (I/O Buffer Information Specification) Modeling discusses various aspects of IBIS including its history, advantages, compatibility, model generation flow, data requirements in modeling the input/output structures and future trends.