SPRSP25A June 2018 – July 2018 TMS320F28035-EP
PRODUCTION DATA.
The default behavior of the GetMode option is to boot to flash. This behavior can be changed to another boot option by programming two locations in the OTP. If the content of either OTP location is invalid, then boot to flash is used. One of the following loaders can be specified: SCI, SPI, I2C, CAN, or OTP.