SPRS357D August 2006 – June 2020 TMS320F28044
PRODUCTION DATA.
Refer to the PDF data sheet for device specific package drawings
It is recommended that the connections for the analog power pins be kept even if the ADC is not used. Following is a summary of how the ADC pins should be connected, if the ADC is not used in an application:
When the ADC is not used, be sure that the clock to the ADC module is not turned on to realize power savings.
When the ADC module is used in an application, unused ADC input pins should be connected to analog ground (VSS1AGND/VSS2AGND)