SPRS902K October 2014 – February 2024 TMS320F28075 , TMS320F28075-Q1 , TMS320F28076
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
In the single-ended mode of operation, a clock signal is connected to X1 with X2 left unconnected. A quartz crystal should not be used in this mode.
In this mode of operation, the clock on X1 is passed to the rest of the chip. See the X1 Input Level Characteristics When Using an External Clock Source (Not a Crystal) table for the input requirements of the buffer.
A single-ended clock may also be connected to GPIO133/AUXCLKIN pin.