(1) This value is based on the flash power-up time, which is a function of the
SYSCLK frequency, flash wait states (RWAIT), and FPAC1[PSLEEP]. For more
information, see the Flash and OTP Power-Down Modes and Wakeup section of the
TMS320F2837xD Dual-Core
Real-Time Microcontrollers Technical Reference Manual
. This value can be
realized when SYSCLK is
200 MHz, RWAIT is
3, and FPAC1[PSLEEP] is 0x860.
A. IDLE instruction is executed to
put the device into HALT mode.
B. The LPM block responds to the
HALT signal, SYSCLK is held for a maximum 16 INTOSC1 clock cycles before being
turned off. This delay enables the CPU pipeline and any other pending operations
to flush properly.
C. Clocks to the peripherals are
turned off and the PLL is shut down. If a quartz crystal or ceramic resonator is
used as the clock source, the internal oscillator is shut down as well. The
device is now in HALT mode and consumes very little power. It is possible to
keep the zero-pin internal oscillators (INTOSC1 and INTOSC2) and the watchdog
alive in HALT MODE. This is done by writing a 1 to CLKSRCCTL1.WDHALTI. After the
IDLE instruction is executed, a delay of five OSCCLK cycles (minimum) is needed
before the wake-up signal could be asserted.
D. When the GPIOn pin (used to bring
the device out of HALT) is driven low, the oscillator is turned on and the
oscillator wakeup sequence is initiated. The GPIO pin should be driven high only
after the oscillator has stabilized. This enables the provision of a clean clock
signal during the PLL lock sequence. Because the falling edge of the GPIO pin
asynchronously begins the wakeup procedure, care should be taken to maintain a
low noise environment prior to entering and during HALT mode.
E. The wake-up signal fed to a GPIO
pin to wake up the device must meet the minimum pulse width requirement.
Furthermore, this signal must be free of glitches. If a noisy signal is fed to a
GPIO pin, the wakeup behavior of the device will not be deterministic and the
device may not exit low-power mode for subsequent wakeup pulses.
F. When CLKIN to the core is
enabled, the device will respond to the interrupt (if enabled), after some
latency. The HALT mode is now exited.
G. Normal operation resumes.
H. The user must relock the PLL upon
HALT wakeup to ensure a stable PLL lock.
Figure 6-23 HALT
Entry and Exit Timing Diagram