SPNS254A June 2022 – March 2024 TMS570LC4357-SEP
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
Table 8-16 lists the event sources that can trigger the conversions for the MibADC1 groups.
| GROUP SOURCE SELECT BITS (G1SRC, G2SRC OR EVSRC) | EVENT NO. | PINMMR161[0] | PINMMR161[1] | CONTROL FOR OPTION A | CONTROL FOR OPTION B | TRIGGER SOURCE |
|---|---|---|---|---|---|---|
| 000 | 1 | x | x | — | — | AD1EVT |
| 001 | 2 | 1 | 0 | PINMMR161[8] = x | PINMMR161[9] = x | N2HET1[8] |
| 0 | 1 | PINMMR161[8] = 1 | PINMMR161[9] = 0 | N2HET2[5] | ||
| 0 | 1 | PINMMR161[8] = 0 | PINMMR161[9] = 1 | e_TPWM_B | ||
| 010 | 3 | 1 | 0 | — | — | N2HET1[10] |
| 0 | 1 | — | — | N2HET1[27] | ||
| 011 | 4 | 1 | 0 | PINMMR161[16] = x | PINMMR161[17] = x | RTI1 Comp0 |
| 0 | 1 | PINMMR161[16] = 1 | PINMMR161[17] = 0 | RTI1 Comp0 | ||
| 0 | 1 | PINMMR161[16] = 0 | PINMMR161[17] = 1 | e_TPWM_A1 | ||
| 100 | 5 | 1 | 0 | — | — | N2HET1[12] |
| 0 | 1 | — | — | N2HET1[17] | ||
| 101 | 6 | 1 | 0 | PINMMR161[24] = x | PINMMR161[25] = x | N2HET1[14] |
| 0 | 1 | PINMMR161[24] = 1 | PINMMR161[25] = 0 | N2HET1[19] | ||
| 0 | 1 | PINMMR161[24] = 0 | PINMMR161[25] = 1 | N2HET2[1] | ||
| 110 | 7 | 1 | 0 | PINMMR162[0] = x | PINMMR162[1] = x | GIOB[0] |
| 0 | 1 | PINMMR162[0] = 1 | PINMMR162[1] = 0 | N2HET1[11] | ||
| 0 | 1 | PINMMR162[0] = 0 | PINMMR162[1] = 1 | ePWM_A2 | ||
| 111 | 8 | 1 | 0 | PINMMR162[8] = x | PINMMR162[9] = x | GIOB[1] |
| 0 | 1 | PINMMR162[8] = 1 | PINMMR162[9] = 0 | N2HET2[13] | ||
| 0 | 1 | PINMMR162[8] = 0 | PINMMR162[9] = 1 | ePWM_AB |
For ADEVT trigger source, the connection to the MibADC1 module trigger input is made from the output side of the input buffer. This way, a trigger condition can be generated either by configuring ADEVT as an output function on to the pad (through the mux control), or by driving the ADEVT signal from an external trigger source as input. If the mux control module is used to select different functionality instead of the ADEVT signal, then care must be taken to disable ADEVT from triggering conversions; there is no multiplexing on the input connection.
If ePWM_B, ePWM_A2, ePWM_AB, N2HET2[1], N2HET2[5], N2HET2[13], N2HET1[11], N2HET1[17], or N2HET1[19] is used to trigger the ADC, the connection to the ADC is made directly from the N2HET or ePWM module outputs. As a result, the ADC can be triggered without having to enable the signal from being output on a device terminal.
For N2HETx trigger sources, the connection to the MibADC1 module trigger input is made from the input side of the output buffer (at the N2HETx module boundary). This way, a trigger condition can be generated even if the N2HETx signal is not selected to be output on the pad.
For the RTI compare 0 interrupt source, the connection is made directly from the output of the RTI module. That is, the interrupt condition can be used as a trigger source even if the actual interrupt is not signaled to the CPU.