SPNS226E June 2013 – November 2016 TMS570LS0714
PRODUCTION DATA.
Refer to the PDF data sheet for device specific package drawings
MIN | MAX | UNIT | ||
---|---|---|---|---|
tpw | Input minimum pulse width | tc(VCLK) + 10(2) | ns | |
tin_slew | Time for input signal to go from VIL to VIH or from VIH to VIL | 1 | ns |
PARAMETER | MIN | MAX | UNIT | |||
---|---|---|---|---|---|---|
Rise time, tr | 8 mA low-EMI pins (see Table 4-40) |
CL = 15 pF | 2.5 | ns | ||
CL = 50 pF | 4 | |||||
CL = 100 pF | 7.2 | |||||
CL = 150 pF | 12.5 | |||||
Fall time, tf | CL = 15 pF | 2.5 | ||||
CL = 50 pF | 4 | |||||
CL = 100 pF | 7.2 | |||||
CL = 150 pF | 12.5 | |||||
Rise time, tr | 4 mA low-EMI pins (see Table 4-40) |
CL = 15 pF | 5.6 | ns | ||
CL = 50 pF | 10.4 | |||||
CL = 100 pF | 16.8 | |||||
CL = 150 pF | 23.2 | |||||
Fall time, tf | CL = 15 pF | 5.6 | ||||
CL= 50 pF | 10.4 | |||||
CL = 100 pF | 16.8 | |||||
CL = 150 pF | 23.2 | |||||
Rise time, tr | 2 mA-z low-EMI pins (see Table 4-40) |
CL = 15 pF | 8 | ns | ||
CL = 50 pF | 15 | |||||
CL = 100 pF | 23 | |||||
CL = 150 pF | 33 | |||||
Fall time, tf | CL = 15 pF | 8 | ||||
CL = 50 pF | 15 | |||||
CL = 100 pF | 23 | |||||
CL = 150 pF | 33 | |||||
Rise time, tr | Selectable 8 mA / 2 mA-z pins (see Table 4-40) |
8mA mode | CL = 15 pF | 2.5 | ns | |
CL = 50 pF | 4 | |||||
CL = 100 pF | 7.2 | |||||
CL = 150 pF | 12.5 | |||||
Fall time, tf | CL = 15 pF | 2.5 | ||||
CL = 50 pF | 4 | |||||
CL = 100 pF | 7.2 | |||||
CL = 150 pF | 12.5 | |||||
Rise time, tr | 2mA-z mode | CL = 15 pF | 8 | |||
CL = 50 pF | 15 | |||||
CL = 100 pF | 23 | |||||
CL = 150 pF | 33 | |||||
Fall time, tf | CL = 15 pF | 8 | ||||
CL = 50 pF | 15 | |||||
CL = 100 pF | 23 | |||||
CL = 150 pF | 33 |
MIN | MAX | UNIT | ||
---|---|---|---|---|
td(parallel_out) | Delay between low-to-high, or high-to-low transition of general-purpose output signals that can be configured by an application in parallel, for example, all signals in a GIOA port, or all N2HET1 signals, and so forth | 6 | ns |
The low-EMI output buffer has been designed explicitly to address the issue of decoupling sources of emissions from the pins which they drive. This is accomplished by adaptively controlling the output buffer impedance, and is particularly effective with capacitive loads.
This is not the default mode of operation of the low-EMI output buffers and must be enabled by setting the system module GPCR1 register for the desired module or signal, as shown in Table 7-4. The adaptive impedance control circuit monitors the DC bias point of the output signal. The buffer internally generates two reference levels, VREFLOW and VREFHIGH, which are set to approximately 10% and 90% of VCCIO, respectively.
Once the output buffer has driven the output to a low level, if the output voltage is below VREFLOW, then the impedance of the output buffer will increase to Hi-Z. A high degree of decoupling between the internal ground bus and the output pin will occur with capacitive loads, or any load in which no current is flowing, for example, the buffer is driving low on a resistive path to ground. Current loads on the buffer which try to pull the output voltage above VREFLOW will be opposed by the impedance of the output buffer so as to maintain the output voltage at or below VREFLOW.
Conversely, once the output buffer has driven the output to a high level, if the output voltage is above VREFHIGH then the output buffer impedance will again increase to Hi-Z. A high degree of decoupling between internal power bus ad output pin will occur with capacitive loads or any loads in which no current is flowing, for example, buffer is driving high on a resistive path to VCCIO. Current loads on the buffer which try to pull the output voltage below VREFHIGH will be opposed by the output buffer impedance so as to maintain the output voltage at or above VREFHIGH.
The bandwidth of the control circuitry is relatively low, so that the output buffer in adaptive impedance control mode cannot respond to high-frequency noise coupling into the power buses of the buffer. In this manner, internal bus noise approaching 20% peak-to-peak of VCCIO can be rejected.
Unlike standard output buffers which clamp to the rails, an output buffer in impedance control mode will allow a positive current load to pull the output voltage up to VCCIO + 0.6V without opposition. Also, a negative current load will pull the output voltage down to VSSIO – 0.6V without opposition. This is not an issue because the actual clamp current capability is always greater than the IOH / IOL specifications.
The low-EMI output buffers are automatically configured to be in the standard buffer mode when the device enters a low-power mode.
MODULE or SIGNAL NAME | LOW-EMI OUTPUT BUFFER SIGNAL HOOKUP | |
---|---|---|
LOW-POWER MODE (LPM) | STANDARD BUFFER ENABLE (SBEN) | |
Module: MibSPI1 | LPM signal from SYS module | GPREG1.0 |
Reserved | GPREG1.1 | |
Module: MibSPI3 | GPREG1.2 | |
Reserved | GPREG1.3 | |
Module: MibSPI5 | GPREG1.4 | |
Reserved | GPREG1.5 | |
Reserved | GPREG1.6 | |
Reserved | GPREG1.7 | |
Signal: TMS | GPREG1.8 | |
Reserved | GPREG1.9 | |
Signal: TDO | GPREG1.10 | |
Signal: RTCK | GPREG1.11 | |
Reserved | GPREG1.12 | |
Signal: nERROR | GPREG1.13 | |
Reserved | GPREG1.14 |
Figure 7-3 shows the connections between the seven ePWM modules (ePWM1–ePWM7) on the device.
Figure 7-4 shows the detailed input synchronization selection (asynchronous, double-synchronous, or double-synchronous + filter width) for ePWMx.
Each ePWM module has a clock enable (EPWMxENCLK). When SYS_nRST is active-low, the clock enables are ignored and the ePWM logic is clocked so that it can reset to a proper state. When SYS_nRST goes in-active high, the state of clock enable is respected.
ePWM MODULE INSTANCE | CONTROL REGISTER TO ENABLE CLOCK |
DEFAULT VALUE |
---|---|---|
ePWM1 | PINMMR37[8] | 1 |
ePWM2 | PINMMR37[16] | 1 |
ePWM3 | PINMMR37[24] | 1 |
ePWM4 | PINMMR38[0] | 1 |
ePWM5 | PINMMR38[8] | 1 |
ePWM6 | PINMMR38[16] | 1 |
ePWM7 | PINMMR38[24] | 1 |
The default value of the control registers to enable the clocks to the ePWMx modules is 1. This means that the VCLK4 clock connections to the ePWMx modules are enabled by default. The application can choose to gate off the VCLK4 clock to any ePWMx module individually by clearing the respective control register bit.
A time-base synchronization scheme connects all of the ePWM modules on a device. Each ePWM module has a synchronization input (EPWMxSYNCI) and a synchronization output (EPWMxSYNCO). The input synchronization for the first instance (ePWM1) comes from an external pin. Figure 7-3 shows the synchronization connections for all the ePWMx modules. Each ePWM module can be configured to use or ignore the synchronization input. For more information, see the ePWM chapter in the device-specific Technical Reference Manual (TRM).
The connection between the N2HET1_LOOP_SYNC and SYNCI input of ePWM1 module is implemented as shown in Figure 7-5.
The TBCLKSYNC bit can be used to globally synchronize the time-base clocks of all enabled ePWM modules on a device. This bit is implemented as PINMMR37 register bit 1.
When TBCLKSYNC = 0, the time-base clock of all ePWM modules is stopped. This is the default condition.
When TBCLKSYNC = 1, all ePWM time-base clocks are started with the rising edge of TBCLK aligned.
For perfectly synchronized TBCLKs, the prescaler bits in the TBCTL register of each ePWM module must be set identically. The proper procedure for enabling the ePWM clocks is as follows:
The output sync from the ePWM1 module is also exported to a device output terminal so that multiple devices can be synchronized together. The signal pulse is stretched by eight VCLK4 cycles before being exported on the terminal as the EPWM1SYNCO signal.
These three trip zone inputs are driven by external circuits and are connected to device-level inputs. These signals are either connected asynchronously to the ePWMx trip zone inputs, or double-synchronized with VCLK4, or double-synchronized and then filtered with a 6-cycle VCLK4-based counter before connecting to the ePWMx (see Figure 7-4). By default, the trip zone inputs are asynchronously connected to the ePWMx modules.
TRIP ZONE INPUT |
CONTROL FOR ASYNCHRONOUS CONNECTION TO ePWMx |
CONTROL FOR DOUBLE-SYNCHRONIZED CONNECTION TO ePWMx |
CONTROL FOR DOUBLE-SYNCHRONIZED AND FILTERED CONNECTION TO ePWMx(1) |
---|---|---|---|
TZ1n | PINMMR46[18:16] = 001 | PINMMR46[18:16] = 010 | PINMMR46[18:16] = 100 |
TZ2n | PINMMR46[26:24] = 001 | PINMMR46[26:24] = 010 | PINMMR46[26:24] = 100 |
TZ3n | PINMMR47[2:0] = 001 | PINMMR47[2:0] = 010 | PINMMR47[2:0] = 100 |
This trip zone input is dedicated to eQEPx error indications. There are two eQEP modules on this device. Each eQEP module indicates a phase error by driving its EQEPxERR output High. The following control registers allow the application to configure the trip zone input (TZ4n) to each ePWMx module based on the requirements of the application.
ePWMx | CONTROL FOR TZ4n = NOT(EQEP1ERR OR EQEP2ERR) |
CONTROL FOR TZ4n = NOT(EQEP1ERR) |
CONTROL FOR TZ4n = NOT(EQEP2ERR) |
---|---|---|---|
ePWM1 | PINMMR41[2:0] = 001 | PINMMR41[2:0] = 010 | PINMMR41[2:0] = 100 |
ePWM2 | PINMMR41[10:8] = 001 | PINMMR41[10:8] = 010 | PINMMR41[10:8] = 100 |
ePWM3 | PINMMR41[18:16] = 001 | PINMMR41[18:16] = 010 | PINMMR41[18:16] = 100 |
ePWM4 | PINMMR41[26:24] = 001 | PINMMR41[26:24] = 010 | PINMMR41[26:24] = 100 |
ePWM5 | PINMMR42[2:0] = 001 | PINMMR42[2:0] = 010 | PINMMR42[2:0] = 100 |
ePWM6 | PINMMR42[10:8] = 001 | PINMMR42[10:8] = 010 | PINMMR42[10:8] = 100 |
ePWM7 | PINMMR42[18:16] = 001 | PINMMR42[18:16] = 010 | PINMMR42[18:16] = 100 |
This trip zone input is dedicated to a clock failure on the device. That is, this trip zone input is asserted whenever an oscillator failure or a PLL slip is detected on the device. The application can use this trip zone input for each ePWMx module to prevent the external system from going out of control when the device clocks are not within expected range (system running at limp clock).
The oscillator failure and PLL slip signals used for this trip zone input are taken from the status flags in the system module. These level signals are set until cleared by the application.
This trip zone input to the ePWMx modules is dedicated to a debug mode entry of the CPU. If enabled, the user can force the PWM outputs to a known state when the emulator stops the CPU. This prevents the external system from going out of control when the CPU is stopped.
A special scheme is implemented to select the actual signal used for triggering the start of conversion on the two ADCs on this device. This scheme is defined in Section 7.5.2.3.
TEST CONDITIONS | MIN | MAX | UNIT | ||
---|---|---|---|---|---|
tw(SYNCIN) | Synchronization input pulse width | Asynchronous | 2 tc(VCLK4) | cycles | |
Synchronous | 2 tc(VCLK4) | ||||
Synchronous, with input filter | 2 tc(VCLK4) + filter width(1) |
PARAMETER | TEST CONDITIONS | MIN | MAX | UNIT | |
---|---|---|---|---|---|
tw(PWM) | Pulse duration, ePWMx output high or low | 33.33 | ns | ||
tw(SYNCOUT) | Synchronization Output Pulse Width | 8 tc(VCLK4) | cycles | ||
td(PWM)tza | Delay time, trip input active to PWM forced high, or Delay time, trip input active to PWM forced low |
No pin load | 25 | ns | |
td(TZ-PWM)HZ | Delay time, trip input active to PWM Hi-Z | 20 | ns |
TEST CONDITIONS | MIN | MAX | UNIT | ||
---|---|---|---|---|---|
tw(TZ) | Pulse duration, TZn input low | Asynchronous | 2 * HSPCLKDIV * CLKDIV * tc(VCLK4)(1) | cycles | |
Synchronous | 2 tc(VCLK4) | ||||
Synchronous, with input filter | 2 tc(VCLK4) + filter width |
Figure 7-6 shows how the eCAP modules are interconnected on this microcontroller.
Figure 7-7 shows the detailed input synchronization selection (asynchronous, double-synchronous, or double-synchronous + filter width) for eCAPx.
Each of the eCAPx modules have a clock enable (ECAPxENCLK). These signals must be generated from a device-level control register. When SYS_nRST is active-low, the clock enables are ignored and the ECAPx logic is clocked so that it can reset to a proper state. When SYS_nRST goes in-active high, the state of clock enable is respected.
eCAP MODULE INSTANCE | CONTROL REGISTER TO ENABLE CLOCK |
DEFAULT VALUE |
---|---|---|
eCAP1 | PINMMR39[0] | 1 |
eCAP2 | PINMMR39[8] | 1 |
eCAP3 | PINMMR39[16] | 1 |
eCAP4 | PINMMR39[24] | 1 |
eCAP5 | PINMMR40[0] | 1 |
eCAP6 | PINMMR40[8] | 1 |
The default value of the control registers to enable the clocks to the eCAPx modules is 1. This means that the VCLK4 clock connections to the eCAPx modules are enabled by default. The application can choose to gate off the VCLK4 clock to any eCAPx module individually by clearing the respective control register bit.
When not used in capture mode, each of the eCAPx modules can be used as a single-channel PWM output. This is called the Auxiliary PWM (APWM) mode of operation of the eCAPx modules. For more information, see the eCAP module chapter of the device-specific TRM.
The input connection to each of the eCAPx modules can be selected between a double-VCLK4-synchronized input or a double-VCLK4-synchronized and filtered input, as shown in Table 7-12.
INPUT SIGNAL | CONTROL FOR DOUBLE-SYNCHRONIZED CONNECTION TO eCAPx |
CONTROL FOR DOUBLE-SYNCHRONIZED AND FILTERED CONNECTION TO eCAPx(1) |
---|---|---|
eCAP1 | PINMMR43[2:0] = 001 | PINMMR43[2:0] = 010 |
eCAP2 | PINMMR43[10:8] = 001 | PINMMR43[10:8] = 010 |
eCAP3 | PINMMR43[18:16] = 001 | PINMMR43[18:16] = 010 |
eCAP4 | PINMMR43[26:24] = 001 | PINMMR43[26:24] = 010 |
eCAP5 | PINMMR44[2:0] = 001 | PINMMR44[2:0] = 010 |
eCAP6 | PINMMR44[10:8] = 001 | PINMMR44[10:8] = 010 |
TEST CONDITIONS | MIN | MAX | UNIT | ||
---|---|---|---|---|---|
tw(CAP) | Pulse width, capture input | Synchronous | 2 tc(VCLK4) | cycles | |
Synchronous with input filter | 2 tc(VCLK4) + filter width(1) |
PARAMETER | TEST CONDITIONS | MIN | MAX | UNIT | |
---|---|---|---|---|---|
tw(APWM) | Pulse duration, APWMx output high or low | 20 | ns |
Figure 7-8 shows the eQEP module interconnections on the device.
Figure 7-9 shows the detailed input synchronization selection (asynchronous, double-synchronous, or double-synchronous + filter width) for eQEPx.
Device-level control registers are implemented to generate the EQEPxENCLK signals. When SYS_nRST is active-low, the clock enables are ignored and the eQEPx logic is clocked so that it can reset to a proper state. When SYS_nRST goes in-active high, the state of clock enable is respected.
The default value of the control registers to enable the clocks to the eQEPx modules is 1 (see Table 7-15). This means that the VCLK4 clock connections to the eQEPx modules are enabled by default. The application can choose to gate off the VCLK4 clock to any eQEPx module individually by clearing the respective control register bit.
The eQEP module sets the EQEPERR signal output whenever a phase error is detected in its inputs EQEPxA and EQEPxB. This error signal from both the eQEP modules is input to the connection selection multiplexer. This multiplexer is defined in Table 7-7. As shown in Figure 7-3, the output of this selection multiplexer is inverted and connected to the TZ4n trip-zone input of all EPWMx modules. This connection allows the application to define the response of each ePWMx module on a phase error indicated by the eQEP modules.
The input connections to each of the eQEP modules can be selected between a double-VCLK4-synchronized input or a double-VCLK4-synchronized and filtered input, as shown in Table 7-16.
INPUT SIGNAL | CONTROL FOR DOUBLE-SYNCHRONIZED CONNECTION TO eQEPx |
CONTROL FOR DOUBLE-SYNCHRONIZED AND FILTERED CONNECTION TO eQEPx(1) |
---|---|---|
eQEP1A | PINMMR44[18:16] = 001 | PINMMR44[18:16] = 010 |
eQEP1B | PINMMR44[26:24] = 001 | PINMMR44[26:24] = 010 |
eQEP1I | PINMMR45[2:0] = 001 | PINMMR45[2:0] = 010 |
eQEP1S | PINMMR45[10:8] = 001 | PINMMR45[10:8] = 010 |
eQEP2A | PINMMR45[18:16] = 001 | PINMMR45[18:16] = 010 |
eQEP2B | PINMMR45[26:24] = 001 | PINMMR45[26:24] = 010 |
eQEP2I | PINMMR46[2:0] = 001 | PINMMR46[2:0] = 010 |
eQEP2S | PINMMR46[10:8] = 001 | PINMMR46[10:8] = 010 |
TEST CONDITIONS | MIN | MAX | UNIT | ||
---|---|---|---|---|---|
tw(QEPP) | QEP input period | Synchronous | 2 tc(VCLK4) | cycles | |
Synchronous with input filter | 2 tc(VCLK4) + filter width | ||||
tw(INDEXH) | QEP Index Input High Time | Synchronous | 2 tc(VCLK4) | cycles | |
Synchronous with input filter | 2 tc(VCLK4) + filter width | ||||
tw(INDEXL) | QEP Index Input Low Time | Synchronous | 2 tc(VCLK4) | cycles | |
Synchronous with input filter | 2 tc(VCLK4) + filter width | ||||
tw(STROBH) | QEP Strobe Input High Time | Synchronous | 2 tc(VCLK4) | cycles | |
Synchronous with input filter | 2 tc(VCLK4) + filter width | ||||
tw(STROBL) | QEP Strobe Input Low Time | Synchronous | 2 tc(VCLK4) | cycles | |
Synchronous with input filter | 2 tc(VCLK4) + filter width |
PARAMETER | MIN | MAX | UNIT | |
---|---|---|---|---|
td(CNTR)xin | Delay time, external clock to counter increment | 4 tc(VCLK4) | cycles | |
td(PCS-OUT)QEP | Delay time, QEP input edge to position compare sync output | 6 tc(VCLK4) | cycles |
The MibADC has a separate power bus for its analog circuitry that enhances the Analog-to-Digital (A-to-D) performance by preventing digital switching noise on the logic circuitry which could be present on VSS and VCC from coupling into the A-to-D analog stage. All A-to-D specifications are given with respect to ADREFLO, unless otherwise noted.
DESCRIPTION | VALUE |
---|---|
Resolution | 12 bits |
Monotonic | Assured |
Output conversion code | 00h to 3FFh [00 for VAI ≤ ADREFLO; 3FFh for VAI ≥ ADREFHI] |
The ADC module supports three conversion groups: Event Group, Group1, and Group2. Each of these three groups can be configured to be triggered by a hardware event. In that case, the application can select the trigger, from among eight event sources, to convert a group.
Table 7-20 lists the event sources that can trigger the conversions for the MibADC1 groups.
GROUP SOURCE SELECT (G1SRC, G2SRC, OR EVSRC) |
EVENT NO. | TRIGGER EVENT SIGNAL | ||||
---|---|---|---|---|---|---|
PINMMR30[0] = 1 (DEFAULT) |
PINMMR30[0] = 0 AND PINMMR30[1] = 1 | |||||
OPTION A | CONTROL FOR OPTION A |
OPTION B | CONTROL FOR OPTION B |
|||
000 | 1 | AD1EVT | AD1EVT | — | AD1EVT | — |
001 | 2 | N2HET1[8] | N2HET2[5] | PINMMR30[8] = 1 | ePWM_B | PINMMR30[8] = 0 and PINMMR30[9] = 1 |
010 | 3 | N2HET1[10] | N2HET1[27] | — | N2HET1[27] | — |
011 | 4 | RTI Compare 0 Interrupt | RTI Compare 0 Interrupt | PINMMR30[16] = 1 | ePWM_A1 | PINMMR30[16] = 0 and PINMMR30[17] = 1 |
100 | 5 | N2HET1[12] | N2HET1[17] | — | N2HET1[17] | — |
101 | 6 | N2HET1[14] | N2HET1[19] | PINMMR30[24] = 1 | N2HET2[1] | PINMMR30[24] = 0 and PINMMR30[25] = 1 |
110 | 7 | GIOB[0] | N2HET1[11] | PINMMR31[0] = 1 | ePWM_A2 | PINMMR31[0] = 0 and PINMMR31[1] = 1 |
111 | 8 | GIOB[1] | N2HET2[13] | PINMMR32[16] = 1 | ePWM_AB | PINMMR31[8] = 0 and PINMMR31[9] = 1 |
NOTE
If ADEVT, N2HET1, or GIOB is used as a trigger source, the connection to the MibADC1 module trigger input is made from the output side of the input buffer. This way, a trigger condition can be generated either by configuring the function as output onto the pad (through the mux control), or by driving the function from an external trigger source as input. If the mux control module is used to select different functionality instead of the ADEVT, N2HET1[x] or GIOB[x] signals, then care must be taken to disable these signals from triggering conversions; there is no multiplexing on the input connections.
If ePWM_B, ePWM_A2, ePWM_AB, N2HET2[1], N2HET2[5], N2HET2[13], N2HET1[11], N2HET1[17], or N2HET1[19] is used to trigger the ADC, the connection to the ADC is made directly from the N2HET or ePWM module outputs. As a result, the ADC can be triggered without having to enable the signal from being output on a device terminal.
NOTE
For the RTI compare 0 interrupt source, the connection is made directly from the output of the RTI module. That is, the interrupt condition can be used as a trigger source even if the actual interrupt is not signaled to the CPU.
Table 7-21 lists the event sources that can trigger the conversions for the MibADC2 groups.
NOTES
If AD2EVT, N2HET1, or GIOB is used as a trigger source, the connection to the MibADC2 module trigger input is made from the output side of the input buffer. This way, a trigger condition can be generated either by configuring the function as output onto the pad (through the mux control), or by driving the function from an external trigger source as input. If the mux control module is used to select different functionality instead of the AD2EVT, N2HET1[x] or GIOB[x] signals, then care must be taken to disable these signals from triggering conversions; there is no multiplexing on the input connections.
If ePWM_B, ePWM_A2, ePWM_AB, N2HET2[1], N2HET2[5], N2HET2[13], N2HET1[11], N2HET1[17], or N2HET1[19] is used to trigger the ADC, the connection to the ADC is made directly from the N2HET or ePWM module outputs. As a result, the ADC can be triggered without having to enable the signal from being output on a device terminal.
NOTE
For the RTI compare 0 interrupt source, the connection is made directly from the output of the RTI module. That is, the interrupt condition can be used as a trigger source even if the actual interrupt is not signaled to the CPU.
As shown in Figure 7-10, the ePWMxSOCA and ePWMxSOCB outputs from each ePWM module are used to generate four signals – ePWM_B, ePWM_A1, ePWM_A2, and ePWM_AB, that are available to trigger the ADC based on the application requirement.
CONTROL BIT | SOC OUTPUT |
---|---|
PINMMR35[0] | SOC1A_SEL |
PINMMR35[8] | SOC2A_SEL |
PINMMR35[16] | SOC3A_SEL |
PINMMR35[24] | SOC4A_SEL |
PINMMR36[0] | SOC5A_SEL |
PINMMR36[8] | SOC6A_SEL |
PINMMR36[16] | SOC7A_SEL |
The SOCA output from each ePWM module is connected to a "switch" shown in Figure 7-10. This switch is implemented by using the control registers in the PINMMR module. Figure 7-11 shows an example of the implementation for the switch on SOC1A. The switches on the other SOCA signals are implemented in the same way.
The logic equations (Equation 1, Equation 2, Equation 3, and Equation 4) for the four outputs from the combinational logic shown in Figure 7-10 are:
PARAMETER | MIN | MAX | UNIT | |
---|---|---|---|---|
ADREFHI | A-to-D high-voltage reference source | ADREFLO | VCCAD(1) | V |
ADREFLO | A-to-D low-voltage reference source | VSSAD(1) | ADREFHI | V |
VAI | Analog input voltage | ADREFLO | ADREFHI | V |
IAIC | Analog input clamp current(2) (VAI < VSSAD – 0.3 or VAI > VCCAD + 0.3) | –2 | 2 | mA |
PARAMETER | DESCRIPTION/CONDITIONS | MIN | MAX | UNIT | ||
---|---|---|---|---|---|---|
Rmux | Analog input mux on-resistance | See Figure 7-12 | 250 | Ω | ||
Rsamp | ADC sample switch on-resistance | See Figure 7-12 | 250 | Ω | ||
Cmux | Input mux capacitance | See Figure 7-12 | 16 | pF | ||
Csamp | ADC sample capacitance | See Figure 7-12 | 13 | pF | ||
IAIL | Analog off-state input leakage current | VCCAD = 3.6 V maximum | VSSAD ≤ VIN < VSSAD + 100 mV | –300 | 200 | nA |
VSSAD + 100 mV ≤ VIN ≤ VCCAD – 200 mV | –200 | 200 | ||||
VCCAD – 200 mV < VIN ≤ VCCAD | –200 | 500 | ||||
IAIL | Analog off-state input leakage current | VCCAD = 5.25 V maximum | VSSAD ≤ VIN < VSSAD + 300 mV | –1000 | 250 | nA |
VSSAD + 300 mV ≤ VIN ≤ VCCAD – 300 mV | –250 | 250 | ||||
VCCAD – 300 mV < VIN ≤ VCCAD | –250 | 1000 | ||||
IAOSB1(1) | ADC1 Analog on-state input bias current | VCCAD = 3.6 V maximum | VSSAD ≤ VIN < VSSAD + 100 mV | –8 | 2 | µA |
VSSAD + 100 mV < VIN < VCCAD – 200 mV | –4 | 2 | ||||
VCCAD – 200 mV < VIN < VCCAD | –4 | 12 | ||||
IAOSB2(1) | ADC2 Analog on-state input bias current | VCCAD = 3.6 V maximum | VSSAD ≤ VIN < VSSAD + 100 mV | –7 | 2 | µA |
VSSAD + 100 mV ≤ VIN ≤ VCCAD – 200 mV | –4 | 2 | ||||
VCCAD - 200 mV < VIN ≤ VCCAD | –4 | 10 | ||||
IAOSB1(1) | ADC1 Analog on-state input bias current | VCCAD = 5.25 V maximum | VSSAD ≤ VIN < VSSAD + 300 mV | –10 | 3 | µA |
VSSAD + 300 mV ≤ VIN ≤ VCCAD – 300 mV | –5 | 3 | ||||
VCCAD – 300 mV < VIN ≤ VCCAD | –5 | 14 | ||||
IAOSB2(1) | ADC2 Analog on-state input bias current | VCCAD = 5.25 V maximum | VSSAD ≤ VIN < VSSAD + 300 mV | –8 | 3 | µA |
VSSAD + 300 mV ≤ VIN ≤ VCCAD – 300 mV | –5 | 3 | ||||
VCCAD – 300 mV < VIN ≤ VCCAD | –5 | 12 | ||||
IADREFHI | ADREFHI input current | ADREFHI = VCCAD, ADREFLO = VSSAD | 3 | mA | ||
ICCAD | Static supply current | Normal operating mode | 15 | mA | ||
ADC core in power down mode | 5 | µA |
PARAMETER | MIN | NOM | MAX | UNIT | |
---|---|---|---|---|---|
tc(ADCLK)(2) | Cycle time, MibADC clock | 0.033 | µs | ||
td(SH)(3) | Delay time, sample and hold time | 0.2 | µs | ||
td(PU-ADV) | Delay time from ADC power on until first input can be sampled | 1 | µs | ||
12-BIT MODE | |||||
td(C) | Delay time, conversion time | 0.4 | µs | ||
td(SHC)(1) | Delay time, total sample/hold and conversion time | 0.6 | µs | ||
10-BIT MODE | |||||
td(C) | Delay time, conversion time | 0.33 | µs | ||
td(SHC)(1) | Delay time, total sample/hold and conversion time | 0.53 | µs |
PARAMETER | DESCRIPTION/CONDITIONS | MIN | NOM | MAX | UNIT | ||
---|---|---|---|---|---|---|---|
CR | Conversion range over which specified accuracy is maintained | ADREFHI – ADREFLO | 3 | 5.25 | V | ||
ZSET | Zero Scale Offset | Difference between the first ideal transition (from code 000h to 001h) and the actual transition | 10-bit mode | 1 | LSB | ||
12-bit mode | 2 | ||||||
FSET | Full Scale Offset | Difference between the range of the measured code transitions (from first to last) and the range of the ideal code transitions | 10-bit mode | 2 | LSB | ||
12-bit mode | 3 | ||||||
EDNL | Differential nonlinearity error | Difference between the actual step width and the ideal value (see Figure 7-13). | 10-bit mode | ± 1.5 | LSB | ||
12-bit mode | ± 2 | ||||||
EINL | Integral nonlinearity error | Maximum deviation from the best straight line through the MibADC. MibADC transfer characteristics, excluding the quantization error. | 10-bit mode | ± 2 | LSB | ||
12-bit mode | ± 2 | ||||||
ETOT | Total unadjusted error | Maximum value of the difference between an analog value and the ideal midstep value. | 10-bit mode | ± 2 | LSB | ||
12-bit mode | ± 4 |
The differential nonlinearity error shown in Figure 7-13 (sometimes referred to as differential linearity) is the difference between an actual step width and the ideal value of 1 LSB.
The integral nonlinearity error shown in Figure 7-14 (sometimes referred to as linearity error) is the deviation of the values on the actual transfer function from a straight line.
The absolute accuracy or total error of an MibADC as shown in Figure 7-15 is the maximum value of the difference between an analog value and the ideal midstep value.
The GPIO module on this device supports two ports, GIOA and GIOB. The I/O pins are bidirectional and bit-programmable. Both GIOA and GIOB support external interrupt capability.
The GPIO module has the following features:
For information on input and output timings see Section 7.1.1 and Section 7.1.2.
The N2HET is an advanced intelligent timer that provides sophisticated timing functions for real-time applications. The timer is software-controlled, using a reduced instruction set, with a specialized timer micromachine and an attached I/O port. The N2HET can be used for pulse width modulated outputs, capture or compare inputs, or general-purpose I/O. The N2HET is especially well suited for applications requiring multiple sensor information and drive actuators with complex and accurate time pulses.
The N2HET module has the following features:
The timer RAM uses four RAM banks, where each bank has two port access capability. This means that one RAM address may be written while another address is read. The RAM words are 96 bits wide, which are split into three 32-bit fields (program, control, and data).
The N2HET instructions PCNT and WCAP impose some timing constraints on the input signals.
PARAMETER | MIN | MAX | UNIT | |
---|---|---|---|---|
1 | Input signal period, PCNT or WCAP for rising edge to rising edge | (HRP) (LRP) tc(VCLK2) + 2 | 225 (HRP) (LRP) tc(VCLK2) – 2 | ns |
2 | Input signal period, PCNT or WCAP for falling edge to falling edge | (HRP) (LRP) tc(VCLK2) + 2 | 225 (HRP) (LRP) tc(VCLK2) – 2 | ns |
3 | Input signal high phase, PCNT or WCAP for rising edge to falling edge | 2 (HRP) tc(VCLK2) + 2 | 225 (HRP) (LRP) tc(VCLK2) – 2 | ns |
4 | Input signal low phase, PCNT or WCAP for falling edge to rising edge | 2 (HRP) tc(VCLK2) + 2 | 225 (HRP) (LRP) tc(VCLK2) – 2 | ns |
In some applications the N2HET resolutions must be synchronized. Some other applications require a single time base to be used for all PWM outputs and input timing captures.
The N2HET provides such a synchronization mechanism. The Clk_master/slave (HETGCR.16) configures the N2HET in master or slave mode (default is slave mode). An N2HET in master mode provides a signal to synchronize the prescalers of the slave N2HET. The slave N2HET synchronizes its loop resolution to the loop resolution signal sent by the master. The slave does not require this signal after it receives the first synchronization signal. However, anytime the slave receives the resynchronization signal from the master, the slave must synchronize itself again.
To assure correctness of the high-end timer operation and output signals, the two N2HET modules can be used to monitor each other’s signals, as shown in Figure 7-18. The direction of the monitoring is controlled by the I/O multiplexing control module.
N2HET1[31] is connected as a clock source for counter 1 in DCC1. This allows the application to measure the frequency of the PWM signal on N2HET1[31].
Similarly, N2HET2[0] is connected as a clock source for counter 1 in DCC2. This allows the application to measure the frequency of the PWM signal on N2HET2[0].
Both N2HET1[31] and N2HET2[0] can be configured to be internal-only channels. That is, the connection to the DCC module is made directly from the output of the N2HETx module (from the input of the output buffer).
For more information on DCC, see Section 6.7.3.
Some applications require disabling the N2HET outputs under some fault condition. The N2HET module provides this capability through the Pin Disable input signal. This signal, when driven low, causes the N2HET outputs identified by a programmable register (HETPINDIS) to be in a high-impedance (tri-state) state. For more details on the N2HET Pin Disable feature, see the device-specific Terminal Reference Manual.
GIOA[5] is connected to the Pin Disable input for N2HET1, and GIOB[2] is connected to the Pin Disable input for N2HET2.
A High-End Timer Transfer Unit (HTU) can perform DMA type transactions to transfer N2HET data to or from main memory. A Memory Protection Unit (MPU) is built into the HET TU.
For the transfer request line trigger connections to the N2HET TU when an instruction-specific condition is true, see Table 7-28 and Table 7-29.
MODULES | REQUEST SOURCE | HET TU1 REQUEST |
---|---|---|
N2HET1 | HTUREQ[0] | HET TU1 DCP[0] |
N2HET1 | HTUREQ[1] | HET TU1 DCP[1] |
N2HET1 | HTUREQ[2] | HET TU1 DCP[2] |
N2HET1 | HTUREQ[3] | HET TU1 DCP[3] |
N2HET1 | HTUREQ[4] | HET TU1 DCP[4] |
N2HET1 | HTUREQ[5] | HET TU1 DCP[5] |
N2HET1 | HTUREQ[6] | HET TU1 DCP[6] |
N2HET1 | HTUREQ[7] | HET TU1 DCP[7] |
MODULES | REQUEST SOURCE | HET TU2 REQUEST |
---|---|---|
N2HET2 | HTUREQ[0] | HET TU2 DCP[0] |
N2HET2 | HTUREQ[1] | HET TU2 DCP[1] |
N2HET2 | HTUREQ[2] | HET TU2 DCP[2] |
N2HET2 | HTUREQ[3] | HET TU2 DCP[3] |
N2HET2 | HTUREQ[4] | HET TU2 DCP[4] |
N2HET2 | HTUREQ[5] | HET TU2 DCP[5] |
N2HET2 | HTUREQ[6] | HET TU2 DCP[6] |
N2HET2 | HTUREQ[7] | HET TU2 DCP[7] |
The DCAN supports the CAN 2.0B protocol standard and uses a serial, multimaster communication protocol that efficiently supports distributed real-time control with robust communication rates of up to 1 Mbps. The DCAN is ideal for applications operating in noisy and harsh environments (for example, automotive and industrial fields) that require reliable serial communication or multiplexed wiring.
Features of the DCAN module include:
For more information on the DCAN, see the device-specific TRM.
PARAMETER | MIN | MAX | UNIT | |
---|---|---|---|---|
td(CANnTX) | Delay time, transmit shift register to CANnTX pin(1) | 15 | ns | |
td(CANnRX) | Delay time, CANnRX pin to receive shift register | 5 | ns |
The SCI/LIN module can be programmed to work either as an SCI or as a LIN. The core of the module is an SCI. The hardware features of the SCI are augmented to achieve LIN compatibility.
The SCI module is a universal asynchronous receiver-transmitter that implements the standard nonreturn to zero (NRZ) format. The SCI can be used to communicate, for example, through an RS-232 port or over a K-line.
The LIN standard is based on the SCI (Universal Asynchronous Receiver/Transmitter [UART]) serial data link format. The communication concept is single-master/multiple-slave with a message identification for multicast transmission between any network nodes.
The following are features of the LIN module:
The I2C module is a multimaster communication module providing an interface between the microcontroller and devices compliant with Philips Semiconductor I2C-bus specification version 2.1 and connected by an I2C-bus. This module will support any slave or master I2C compatible device.
The I2C module has the following features:
NOTE
This I2C module does not support:
PARAMETER | STANDARD MODE | FAST MODE | UNIT | |||
---|---|---|---|---|---|---|
MIN | MAX | MIN | MAX | |||
tc(I2CCLK) | Cycle time, internal module clock for I2C, prescaled from VCLK | 75.2 | 149 | 75.2 | 149 | ns |
f(SCL) | SCL clock frequency | 0 | 100 | 0 | 400 | kHz |
tc(SCL) | Cycle time, SCL | 10 | 2.5 | µs | ||
tsu(SCLH-SDAL) | Setup time, SCL high before SDA low (for a repeated START condition) | 4.7 | 0.6 | µs | ||
th(SCLL-SDAL) | Hold time, SCL low after SDA low (for a repeated START condition) | 4 | 0.6 | µs | ||
tw(SCLL) | Pulse duration, SCL low | 4.7 | 1.3 | µs | ||
tw(SCLH) | Pulse duration, SCL high | 4 | 0.6 | µs | ||
tsu(SDA-SCLH) | Setup time, SDA valid before SCL high | 250 | 100 | ns | ||
th(SDA-SCLL) | Hold time, SDA valid after SCL low (for I2C-bus devices) | 0 | 3.45(2) | 0 | 0.9 | µs |
tw(SDAH) | Pulse duration, SDA high between STOP and START conditions | 4.7 | 1.3 | µs | ||
tsu(SCLH-SDAH) | Setup time, SCL high before SDA high (for STOP condition) | 4.0 | 0.6 | µs | ||
tw(SP) | Pulse duration, spike (must be suppressed) | 0 | 50 | ns | ||
Cb(3) | Capacitive load for each bus line | 400 | 400 | pF |
NOTE
The MibSPI is a high-speed synchronous serial I/O port that allows a serial bit stream of programmed length (2 to 16 bits) to be shifted in and out of the device at a programmed bit-transfer rate. Typical applications for the SPI include interfacing to external peripherals, such as I/Os, memories, display drivers, and ADCs.
Both standard and MibSPI modules have the following features:
The multibuffer RAM is comprised of 128 buffers. Each entry in the multibuffer RAM consists of four parts: a 16-bit transmit field, a 16-bit receive field, a 16-bit control field, and a 16-bit status field. The multibuffer RAM can be partitioned into multiple transfer group with variable number of buffers each. Each MibSPIx module supports eight transfer groups.
Each transfer group can be configured individually. For each transfer group, a trigger event and a trigger source can be chosen. A trigger event can be for example a rising edge or a permanent low level at a selectable trigger source. For example, up to 15 trigger sources are available which can be used by each transfer group. These trigger options are listed in Table 7-33 and Section 7.12.3.2 for MibSPI1 and MibSPI3, respectively.
EVENT NO. | TGxCTRL TRIGSRC[3:0] | TRIGGER |
---|---|---|
Disabled | 0000 | No trigger source |
EVENT0 | 0001 | GIOA[0] |
EVENT1 | 0010 | GIOA[1] |
EVENT2 | 0011 | GIOA[2] |
EVENT3 | 0100 | GIOA[3] |
EVENT4 | 0101 | GIOA[4] |
EVENT5 | 0110 | GIOA[5] |
EVENT6 | 0111 | GIOA[6] |
EVENT7 | 1000 | GIOA[7] |
EVENT8 | 1001 | N2HET1[8] |
EVENT9 | 1010 | N2HET1[10] |
EVENT10 | 1011 | N2HET1[12] |
EVENT11 | 1100 | N2HET1[14] |
EVENT12 | 1101 | N2HET1[16] |
EVENT13 | 1110 | N2HET1[18] |
EVENT14 | 1111 | Intern Tick counter |
NOTE
For N2HET1 trigger sources, the connection to the MibSPI1 module trigger input is made from the input side of the output buffer (at the N2HET1 module boundary). This way, a trigger condition can be generated even if the N2HET1 signal is not selected to be output on the pad.
NOTE
For GIOx trigger sources, the connection to the MibSPI1 module trigger input is made from the output side of the input buffer. This way, a trigger condition can be generated either by selecting the GIOx pin as an output pin and selecting the pin to be a GIOx pin, or by driving the GIOx pin from an external trigger source. If the mux control module is used to select different functionality instead of the GIOx signal, then care must be taken to disable GIOx from triggering MibSPI1 transfers; there is no multiplexing on the input connections.
EVENT NO. | TGxCTRL TRIGSRC[3:0] | TRIGGER |
---|---|---|
Disabled | 0000 | No trigger source |
EVENT0 | 0001 | GIOA[0] |
EVENT1 | 0010 | GIOA[1] |
EVENT2 | 0011 | GIOA[2] |
EVENT3 | 0100 | GIOA[3] |
EVENT4 | 0101 | GIOA[4] |
EVENT5 | 0110 | GIOA[5] |
EVENT6 | 0111 | GIOA[6] |
EVENT7 | 1000 | GIOA[7] |
EVENT8 | 1001 | N2HET1[8] |
EVENT9 | 1010 | N2HET1[10] |
EVENT10 | 1011 | N2HET1[12] |
EVENT11 | 1100 | N2HET1[14] |
EVENT12 | 1101 | N2HET1[16] |
EVENT13 | 1110 | N2HET1[18] |
EVENT14 | 1111 | Intern Tick counter |
NOTE
For N2HET1 trigger sources, the connection to the MibSPI3 module trigger input is made from the input side of the output buffer (at the N2HET1 module boundary). This way, a trigger condition can be generated even if the N2HET1 signal is not selected to be output on the pad.
NOTE
For GIOx trigger sources, the connection to the MibSPI3 module trigger input is made from the output side of the input buffer. This way, a trigger condition can be generated either by selecting the GIOx pin as an output pin and selecting the pin to be a GIOx pin, or by driving the GIOx pin from an external trigger source. If the mux control module is used to select different functionality instead of the GIOx signal, then care must be taken to disable GIOx from triggering MibSPI3 transfers; there is no multiplexing on the input connections.
EVENT NO. | TGxCTRL TRIGSRC[3:0] | TRIGGER |
---|---|---|
Disabled | 0000 | No trigger source |
EVENT0 | 0001 | GIOA[0] |
EVENT1 | 0010 | GIOA[1] |
EVENT2 | 0011 | GIOA[2] |
EVENT3 | 0100 | GIOA[3] |
EVENT4 | 0101 | GIOA[4] |
EVENT5 | 0110 | GIOA[5] |
EVENT6 | 0111 | GIOA[6] |
EVENT7 | 1000 | GIOA[7] |
EVENT8 | 1001 | N2HET1[8] |
EVENT9 | 1010 | N2HET1[10] |
EVENT10 | 1011 | N2HET1[12] |
EVENT11 | 1100 | N2HET1[14] |
EVENT12 | 1101 | N2HET1[16] |
EVENT13 | 1110 | N2HET1[18] |
EVENT14 | 1111 | Intern Tick counter |
NOTE
For N2HET1 trigger sources, the connection to the MibSPI5 module trigger input is made from the input side of the output buffer (at the N2HET1 module boundary). This way, a trigger condition can be generated even if the N2HET1 signal is not selected to be output on the pad.
NOTE
For GIOx trigger sources, the connection to the MibSPI5 module trigger input is made from the output side of the input buffer. This way, a trigger condition can be generated either by selecting the GIOx pin as an output pin and selecting the pin to be a GIOx pin, or by driving the GIOx pin from an external trigger source. If the mux control module is used to select different functionality instead of the GIOx signal, then care must be taken to disable GIOx from triggering MibSPI5 transfers; there is no multiplexing on the input connections.
NO. | PARAMETER | MIN | MAX | UNIT | ||
---|---|---|---|---|---|---|
1 | tc(SPC)M | Cycle time, SPICLK(4) | 40 | 256tc(VCLK) | ns | |
2(5) | tw(SPCH)M | Pulse duration, SPICLK high (clock polarity = 0) | 0.5tc(SPC)M – tr(SPC)M – 3 | 0.5tc(SPC)M + 3 | ns | |
tw(SPCL)M | Pulse duration, SPICLK low (clock polarity = 1) | 0.5tc(SPC)M – tf(SPC)M – 3 | 0.5tc(SPC)M + 3 | |||
3(5) | tw(SPCL)M | Pulse duration, SPICLK low (clock polarity = 0) | 0.5tc(SPC)M – tf(SPC)M – 3 | 0.5tc(SPC)M + 3 | ns | |
tw(SPCH)M | Pulse duration, SPICLK high (clock polarity = 1) | 0.5tc(SPC)M – tr(SPC)M – 3 | 0.5tc(SPC)M + 3 | |||
4(5) | td(SPCH-SIMO)M | Delay time, SPISIMO valid before SPICLK low (clock polarity = 0) | 0.5tc(SPC)M – 6 | ns | ||
td(SPCL-SIMO)M | Delay time, SPISIMO valid before SPICLK high (clock polarity = 1) | 0.5tc(SPC)M – 6 | ||||
5(5) | tv(SPCL-SIMO)M | Valid time, SPISIMO data valid after SPICLK low (clock polarity = 0) | 0.5tc(SPC)M – tf(SPC) – 4 | ns | ||
tv(SPCH-SIMO)M | Valid time, SPISIMO data valid after SPICLK high (clock polarity = 1) | 0.5tc(SPC)M – tr(SPC) – 4 | ||||
6(5) | tsu(SOMI-SPCL)M | Setup time, SPISOMI before SPICLK low (clock polarity = 0) | tf(SPC) + 2.2 | ns | ||
tsu(SOMI-SPCH)M | Setup time, SPISOMI before SPICLK high (clock polarity = 1) | tr(SPC) + 2.2 | ||||
7(5) | th(SPCL-SOMI)M | Hold time, SPISOMI data valid after SPICLK low (clock polarity = 0) | 10 | ns | ||
th(SPCH-SOMI)M | Hold time, SPISOMI data valid after SPICLK high (clock polarity = 1) | 10 | ||||
8(6) | tC2TDELAY | Setup time CS active until SPICLK high (clock polarity = 0) | CSHOLD = 0 | C2TDELAY*tc(VCLK) + 2*tc(VCLK) - tf(SPICS) + tr(SPC) – 7 | (C2TDELAY+2) * tc(VCLK) - tf(SPICS) + tr(SPC) + 5.5 | ns |
CSHOLD = 1 | C2TDELAY*tc(VCLK) + 3*tc(VCLK) - tf(SPICS) + tr(SPC) – 7 | (C2TDELAY+3) * tc(VCLK) - tf(SPICS) + tr(SPC) + 5.5 | ||||
Setup time CS active until SPICLK low (clock polarity = 1) | CSHOLD = 0 | C2TDELAY*tc(VCLK) + 2*tc(VCLK) - tf(SPICS) + tf(SPC) – 7 | (C2TDELAY+2) * tc(VCLK) - tf(SPICS) + tf(SPC) + 5.5 | |||
CSHOLD = 1 | C2TDELAY*tc(VCLK) + 3*tc(VCLK) - tf(SPICS) + tf(SPC) – 7 | (C2TDELAY+3) * tc(VCLK) - tf(SPICS) + tf(SPC) + 5.5 | ||||
9(6) | tT2CDELAY | Hold time SPICLK low until CS inactive (clock polarity = 0) | 0.5*tc(SPC)M + T2CDELAY*tc(VCLK) + tc(VCLK) - tf(SPC) + tr(SPICS) - 7 | 0.5*tc(SPC)M + T2CDELAY*tc(VCLK) + tc(VCLK) - tf(SPC) + tr(SPICS) + 11 | ns | |
Hold time SPICLK high until CS inactive (clock polarity = 1) | 0.5*tc(SPC)M + T2CDELAY*tc(VCLK) + tc(VCLK) - tr(SPC) + tr(SPICS) - 7 | 0.5*tc(SPC)M + T2CDELAY*tc(VCLK) + tc(VCLK) - tr(SPC) + tr(SPICS) + 11 | ||||
10 | tSPIENA | SPIENAn Sample point | (C2TDELAY+1) * tc(VCLK) - tf(SPICS) – 29 | (C2TDELAY+1)*tc(VCLK) | ns | |
11 | tSPIENAW | SPIENAn Sample point from write to buffer | (C2TDELAY+2)*tc(VCLK) | ns |
NO. | PARAMETER | MIN | MAX | UNIT | ||
---|---|---|---|---|---|---|
1 | tc(SPC)M | Cycle time, SPICLK (4) | 40 | 256tc(VCLK) | ns | |
2(5) | tw(SPCH)M | Pulse duration, SPICLK high (clock polarity = 0) | 0.5tc(SPC)M – tr(SPC)M – 3 | 0.5tc(SPC)M + 3 | ns | |
tw(SPCL)M | Pulse duration, SPICLK low (clock polarity = 1) | 0.5tc(SPC)M – tf(SPC)M – 3 | 0.5tc(SPC)M + 3 | |||
3(5) | tw(SPCL)M | Pulse duration, SPICLK low (clock polarity = 0) | 0.5tc(SPC)M – tf(SPC)M – 3 | 0.5tc(SPC)M + 3 | ns | |
tw(SPCH)M | Pulse duration, SPICLK high (clock polarity = 1) | 0.5tc(SPC)M – tr(SPC)M – 3 | 0.5tc(SPC)M + 3 | |||
4(5) | tv(SIMO-SPCH)M | Valid time, SPICLK high after SPISIMO data valid (clock polarity = 0) | 0.5tc(SPC)M – 6 | ns | ||
tv(SIMO-SPCL)M | Valid time, SPICLK low after SPISIMO data valid (clock polarity = 1) | 0.5tc(SPC)M – 6 | ||||
5(5) | tv(SPCH-SIMO)M | Valid time, SPISIMO data valid after SPICLK high (clock polarity = 0) | 0.5tc(SPC)M – tr(SPC) – 4 | ns | ||
tv(SPCL-SIMO)M | Valid time, SPISIMO data valid after SPICLK low (clock polarity = 1) | 0.5tc(SPC)M – tf(SPC) – 4 | ||||
6(5) | tsu(SOMI-SPCH)M | Setup time, SPISOMI before SPICLK high (clock polarity = 0) | tr(SPC)+ 2.2 | ns | ||
tsu(SOMI-SPCL)M | Setup time, SPISOMI before SPICLK low (clock polarity = 1) | tf(SPC)+ 2.2 | ||||
7(5) | tv(SPCH-SOMI)M | Valid time, SPISOMI data valid after SPICLK high (clock polarity = 0) | 10 | ns | ||
tv(SPCL-SOMI)M | Valid time, SPISOMI data valid after SPICLK low (clock polarity = 1) | 10 | ||||
8(6) | tC2TDELAY | Setup time CS active until SPICLK high (clock polarity = 0) | CSHOLD = 0 | 0.5*tc(SPC)M + (C2TDELAY+2) * tc(VCLK) - tf(SPICS) + tr(SPC) – 7 |
0.5*tc(SPC)M + (C2TDELAY+2) * tc(VCLK) - tf(SPICS) + tr(SPC) + 5.5 |
ns |
CSHOLD = 1 | 0.5*tc(SPC)M + (C2TDELAY+3) * tc(VCLK) - tf(SPICS) + tr(SPC) – 7 |
0.5*tc(SPC)M + (C2TDELAY+3) * tc(VCLK) - tf(SPICS) + tr(SPC) + 5.5 |
||||
Setup time CS active until SPICLK low (clock polarity = 1) | CSHOLD = 0 | 0.5*tc(SPC)M + (C2TDELAY+2) * tc(VCLK) - tf(SPICS) + tf(SPC) – 7 |
0.5*tc(SPC)M + (C2TDELAY+2) * tc(VCLK) - tf(SPICS) + tf(SPC) + 5.5 |
|||
CSHOLD = 1 | 0.5*tc(SPC)M + (C2TDELAY+3) * tc(VCLK) - tf(SPICS) + tf(SPC) – 7 |
0.5*tc(SPC)M + (C2TDELAY+3) * tc(VCLK) - tf(SPICS) + tf(SPC) + 5.5 |
||||
9(6) | tT2CDELAY | Hold time SPICLK low until CS inactive (clock polarity = 0) | T2CDELAY*tc(VCLK) + tc(VCLK) - tf(SPC) + tr(SPICS) - 7 |
T2CDELAY*tc(VCLK) + tc(VCLK) - tf(SPC) + tr(SPICS) + 11 |
ns | |
Hold time SPICLK high until CS inactive (clock polarity = 1) | T2CDELAY*tc(VCLK) + tc(VCLK) - tr(SPC) + tr(SPICS) - 7 |
T2CDELAY*tc(VCLK) + tc(VCLK) - tr(SPC) + tr(SPICS) + 11 |
||||
10 | tSPIENA | SPIENAn Sample Point | (C2TDELAY+1)* tc(VCLK) - tf(SPICS) – 29 | (C2TDELAY+1)*tc(VCLK) | ns | |
11 | tSPIENAW | SPIENAn Sample point from write to buffer | (C2TDELAY+2)*tc(VCLK) | ns |
NO. | PARAMETER | MIN | MAX | UNIT | |
---|---|---|---|---|---|
1 | tc(SPC)S | Cycle time, SPICLK(5) | 40 | ns | |
2(6) | tw(SPCH)S | Pulse duration, SPICLK high (clock polarity = 0) | 14 | ns | |
tw(SPCL)S | Pulse duration, SPICLK low (clock polarity = 1) | 14 | |||
3(6) | tw(SPCL)S | Pulse duration, SPICLK low (clock polarity = 0) | 14 | ns | |
tw(SPCH)S | Pulse duration, SPICLK high (clock polarity = 1) | 14 | |||
4(6) | td(SPCH-SOMI)S | Delay time, SPISOMI valid after SPICLK high (clock polarity = 0) | trf(SOMI) + 20 | ns | |
td(SPCL-SOMI)S | Delay time, SPISOMI valid after SPICLK low (clock polarity = 1) | trf(SOMI) + 20 | |||
5(6) | th(SPCH-SOMI)S | Hold time, SPISOMI data valid after SPICLK high (clock polarity =0) | 2 | ns | |
th(SPCL-SOMI)S | Hold time, SPISOMI data valid after SPICLK low (clock polarity =1) | 2 | |||
6(6) | tsu(SIMO-SPCL)S | Setup time, SPISIMO before SPICLK low (clock polarity = 0) | 4 | ns | |
tsu(SIMO-SPCH)S | Setup time, SPISIMO before SPICLK high (clock polarity = 1) | 4 | |||
7(6) | th(SPCL-SIMO)S | Hold time, SPISIMO data valid after SPICLK low (clock polarity = 0) | 2 | ns | |
th(SPCH-SIMO)S | Hold time, SPISIMO data valid after S PICLK high (clock polarity = 1) | 2 | |||
8 | td(SPCL-SENAH)S | Delay time, SPIENAn high after last SPICLK low (clock polarity = 0) | 1.5tc(VCLK) | 2.5tc(VCLK)+tr(ENAn)+22 | ns |
td(SPCH-SENAH)S | Delay time, SPIENAn high after last SPICLK high (clock polarity = 1) | 1.5tc(VCLK) | 2.5tc(VCLK)+tr(ENAn)+22 | ||
9 | td(SCSL-SENAL)S | Delay time, SPIENAn low after SPICSn low (if new data has been written to the SPI buffer) | tf(ENAn) | tc(VCLK)+tf(ENAn)+27 | ns |
NO. | PARAMETER | MIN | MAX | UNIT | |
---|---|---|---|---|---|
1 | tc(SPC)S | Cycle time, SPICLK(5) | 40 | ns | |
2(6) | tw(SPCH)S | Pulse duration, SPICLK high (clock polarity = 0) | 14 | ns | |
tw(SPCL)S | Pulse duration, SPICLK low (clock polarity = 1) | 14 | |||
3(6) | tw(SPCL)S | Pulse duration, SPICLK low (clock polarity = 0) | 14 | ns | |
tw(SPCH)S | Pulse duration, SPICLK high (clock polarity = 1) | 14 | |||
4(6) | td(SOMI-SPCL)S | Delay time, SPISOMI data valid after SPICLK low (clock polarity = 0) | trf(SOMI) + 20 | ns | |
td(SOMI-SPCH)S | Delay time, SPISOMI data valid after SPICLK high (clock polarity = 1) | trf(SOMI) + 20 | |||
5(6) | th(SPCL-SOMI)S | Hold time, SPISOMI data valid after SPICLK high (clock polarity =0) | 2 | ns | |
th(SPCH-SOMI)S | Hold time, SPISOMI data valid after SPICLK low (clock polarity =1) | 2 | |||
6(6) | tsu(SIMO-SPCH)S | Setup time, SPISIMO before SPICLK high (clock polarity = 0) | 4 | ns | |
tsu(SIMO-SPCL)S | Setup time, SPISIMO before SPICLK low (clock polarity = 1) | 4 | |||
7(6) | tv(SPCH-SIMO)S | High time, SPISIMO data valid after SPICLK high (clock polarity = 0) | 2 | ns | |
tv(SPCL-SIMO)S | High time, SPISIMO data valid after SPICLK low (clock polarity = 1) | 2 | |||
8 | td(SPCH-SENAH)S | Delay time, SPIENAn high after last SPICLK high (clock polarity = 0) | 1.5tc(VCLK) | 2.5tc(VCLK)+tr(ENAn)+22 | ns |
td(SPCL-SENAH)S | Delay time, SPIENAn high after last SPICLK low (clock polarity = 1) | 1.5tc(VCLK) | 2.5tc(VCLK)+tr(ENAn)+22 | ||
9 | td(SCSL-SENAL)S | Delay time, SPIENAn low after SPICSn low (if new data has been written to the SPI buffer) | tf(ENAn) | tc(VCLK)+tf(ENAn)
+27 |
ns |
10 | td(SCSL-SOMI)S | Delay time, SOMI valid after SPICSn low (if new data has been written to the SPI buffer) | tc(VCLK) | 2tc(VCLK)+trf(SOMI)+28 | ns |