SCDS393A April 2019 – October 2019 TMUX1204
PRODUCTION DATA.
The TMUX1204 has a transmission-gate topology. Any mismatch in capacitance between the NMOS and PMOS transistors results in a charge injected into the drain or source during the falling or rising edge of the gate signal. The amount of charge injected into the source or drain of the device is known as charge injection, and is denoted by the symbol QC. Figure 13 shows the setup used to measure charge injection from source (Sx) to drain (D).