SCDS376A February 2018 – September 2018 TMUX6104
PRODUCTION DATA.
The TMUX6104 have a simple transmission-gate topology. Any mismatch in capacitance between the NMOS and PMOS transistors results in a charge injected into the drain or source during the falling or rising edge of the gate signal. The amount of charge injected into the source or drain of the device is known as charge injection, and is denoted by the symbol QINJ. Figure 23 shows the setup used to measure charge injection from source (Sx) to drain (D).