SCDS397A November 2018 – October 2022 TMUX6136
PRODUCTION DATA
The on-resistance of the TMUX6136 is the ohmic resistance across the source (Sx) and drain (D) pins of the device. The on-resistance varies with input voltage and supply voltage. The symbol RON is used to denote on-resistance. The measurement setup used to measure RON is shown in Figure 7-1. Voltage (V) and current (ICH) are measured using this setup, and RON is computed as shown in Equation 1.