SCDS450A November 2022 – March 2023 TMUX6201 , TMUX6202
PRODUCTION DATA
One application of the TMUX620x is to configure the feedback on a discrete transimpedance amplifier (TIA) implementation. Often, TIAs are used in applications such as photodiode inputs, which then feeds into an ADC or MCU/processor. Depending on the expected strength of the photodiode input, and the needed accuracy, multiple gain levels are needed. A switch like the TMUX620x allows for different gain values to be selected, changing the level of amplifications. This solution can be scaled, but as much as needed for multiple gain options.
Figure 10-1 shows the TMUX620x configured with a precision op amp to enable multiple gains.