The following are two types of
crosstalk that can be defined for the devices:
- Intra-channel crosstalk (XTALK(INTRA)): the voltage
at the source pin (Sx) of an off-switch input, when a 1-VRMS signal
is applied at the source pin of an on-switch input in the same channel, as shown
in Figure 8-13.
- Inter-channel crosstalk (XTALK(INTER)): the voltage
at the source pin (Sx) of an on-switch input, when a 1-VRMS signal is
applied at the source pin of an on-switch input in a different channel, as shown
in Figure 8-14. Inter-channel crosstalk applies only to the TMUX7309F device.