SCDS459A October 2022 – November 2022 TMUX7436F
PRODMIX
tON(EN) is defined as the time taken by the output of the TMUX7436F to rise to a 90% final value after the EN signal has past the 50% threshold. tOFF(EN) is defined as the time taken by the output of the TMUX7436F to fall to a 10% initial value after the EN signal has past the 50% threshold. Figure 7-6 shows the setup used to measure tON and tOFF.