SCDS394B march 2021 – june 2023 TMUX7462F
PRODUCTION DATA
Bandwidth (BW) is defined as the range of frequencies that are attenuated by < 3 dB when the input is applied to the source pin (Sx) of an on-channel, and the output is measured at the TMUX7462F's drain pin (D or Dx). Figure 7-11 and Equation 2 shows the setup used to measure bandwidth of the switch.