Use an unbroken ground plane to have good low impedance and inductance return path to the power supply for power and audio signals.
Maintain a contiguous ground plane from the ground pins to the PCB area surrounding the device for as many of the ground pins as possible, since the ground pins are the best conductors of heat in the package.
PCB layout, audio performance and EMI are linked closely together.
Routing the audio input should be kept short and together with the accompanied audio source ground.
The small bypass capacitors on the PVDD lines of the DUT be placed as close the PVDD pins as possible.
A local ground area underneath the device is important to keep solid to minimize ground bounce.
Orient the passive component so that the narrow end of the passive component is facing the TPA3250 device, unless the area between two pads of a passive component is large enough to allow copper to flow in between the two pads.
Avoid placing other heat producing components or structures near the TPA3250 device.
Avoid cutting off the flow of heat from the TPA3250 device to the surrounding ground areas with traces or via strings, especially on output side of device.
Netlist for this printed circuit board is generated from the schematic in Figure 32.
12.2 Layout Examples
12.2.1 BTL Application Printed Circuit Board Layout Example
A. Note: PCB layout example shows composite layout. Dark grey: Top layer copper traces, light gray: Bottom layer copper traces. All PCB area not used for traces should be GND copper pour (transparent on example image)
B. Note T1: PVDD decoupling bulk capacitors should be as close as possible to the PVDD and GND_X pins. Wide traces should be routed on the top layer with direct connection to the pins and without going through vias. No vias or traces should be blocking the current path.
C. Note T2: Close decoupling of PVDD with low impedance X7R ceramic capacitors placed close to the pins.
D. Note T3: PowerPad™ needs to be soldered to PCB GND copper pour
12.2.2 SE Application Printed Circuit Board Layout Example
A. Note: PCB layout example shows composite layout. Dark grey: Top layer copper traces, light gray: Bottom layer copper traces. All PCB area not used for traces should be GND copper pour (transparent on example image)
B. Note T1: PVDD decoupling bulk capacitors should be as close as possible to the PVDD and GND_X pins. Wide traces should be routed on the top layer with direct connection to the pins and without going through vias. No vias or traces should be blocking the current path.
C. Note T2: Close decoupling of PVDD with low impedance X7R ceramic capacitors is placed close to the pins.
D. Note T3: PowerPad™ needs to be soldered to PCB GND copper pour
Figure 33. SE Application Printed Circuit Board - Composite
12.2.3 PBTL Application Printed Circuit Board Layout Example
A. Note: PCB layout example shows composite layout. Dark grey: Top layer copper traces, light gray: Bottom layer copper traces. All PCB area not used for traces should be GND copper pour (transparent on example image)
B. Note T1: PVDD decoupling bulk capacitors should be as close as possible to the PVDD and GND_X pins. Wide traces should be routed on the top layer with direct connection to the pins and without going through vias. No vias or traces should be blocking the current path.
C. Note T2: Close decoupling of PVDD with low impedance X7R ceramic capacitors is placed close to the pins.
D. ote T3: PowerPad™ needs to be soldered to PCB GND copper pour