SLASEP6B September 2019 – December 2020 TPA6304-Q1
PRODUCTION DATA
If the output load current reaches over current shutdown threshold, ISD, such as during an output short to GND or power supply, then an Over Current Shut Down (OCSD) Event occurs which limits the peak current and shuts down the affected channel. There are four programmable OC levels that determine ISD. These can be set in Miscellaneous Control Register 1. The time to shutdown the channel varies depending on the severity of the short condition. The channel is placed into the PROTECTIVE SHUTDOWN State, the output stage is high impedance.
Based on the default configuration a fault signal is generated which by default generates an active low signal at the FAULT Pin.