SLASEP6B September 2019 – December 2020 TPA6304-Q1
PRODUCTION DATA
The device has the capability of placing two channels into a parallel configuration that allows for twice the current drive capability for low impedance loads. BTL and PBTL modes can be me mixed. Channels 1 and 2 can be placed in PBTL, channels 3 and 4 can be placed into PBTL, or both pairs can be placed in PBTL. Follow the Typical application schematic for proper input and output connections for PBTL configuration useing both pairs. The speaker output connections must be made on the speaker side of the LC filter. The device can drive more current with paralleling BTL channels on the load side of the LC output filter. The input connections on channel 2 and channel 4 should be connected to ground.
The Mode Control Register has to be set for PBTL operations. Bit 4 sets channels 1 and 2 to PBTL and Bit 5 sets channels 3 and 4 to PBTL. These bits must only be changed while the STANDBY pin is asserted low.
Load diagnostics is supported for PBTL channels.