SCPS287B November 2023 – December 2024 TPLD1201
PRODUCTION DATA
When CNT/DLY3 is configured as a Delay, this macro-cell has the option to generate a pulse of approximately 20ns width when a valid edge is detected. The edge on which the Edge detector generates a pulse is determined by the Edge select parameter and can be configured as:
Rising: only rising edges of IN generate a pulse.
Falling: only falling edges of IN generate a pulse.
Both: both rising and falling edges of IN generate a pulse.
The image below shows an example of how the EDET option operates with respect to the Edge select parameter.