SCPS301 September 2024 TPLD801-Q1
ADVANCE INFORMATION
The TPLD801-Q1 contains one-time programmable (OTP) non-volatile memory, which retain the device configuration in the absence of a power supply. Once a POR event is issued to the device, the OTP content is loaded into the macro-cells per the POR sequence shown in Section 7.4.1.
The TPLD801-Q1 OTP memory can be emulated for quick in-system evaluation or permanently burned using the TPLD801-Q1 EVM and InterConnect Studio software platform. While emulating the OTP, the TPLD will keep its programmed configuration as long as the supply power is provided. Once a power cycle is issued, the TPLD will revert to the configuration stored in the OTP.