SLVSG57 August 2021 TPS1653
PRODUCTION DATA
The Undervoltage Lockout (UVLO) trip point are adjusted using an external voltage divider network of R1 and R2 connected between IN, UVLO, and GND pins of the device. The values required for setting the undervoltage are calculated by solving V(UVLOR) = R2 / (R1+R2) × V(UV_IN).
For minimizing the input current drawn from the power supply, {I(R12) = V(IN) / (R1 + R2 )}, TI recommends to use higher value resistance for R1 and R2.
However, the leakage current due to external active components connected at resistor string can add error to these calculations. So, the resistor string current, I(R12) must be chosen to be 20 times greater than the leakage current of UVLO pin.
Choose the closest standard 1% resistor values: R1 = 887 kΩ, R2 = 63.4 kΩ.