Locate all the TPS1663x family support components R(ILIM), R(PLIM), C(dVdT), R(IMON), UVLO, OVP resistors close to their connection pin. Connect the other end of the component to the GND with shortest trace length.
The trace routing for the R(ILIM), R(PLIM) component to the device must be as short as possible to reduce parasitic effects on the current limit and power limit accuracy. These traces must not have any coupling to switching signals on the board.
Protection devices such as TVS, snubbers,
capacitors, or diodes must be placed physically close to the device they are
intended to protect, and routed with short traces to reduce inductance. For
example, TI recommends a protection Schottky diode to address negative
transients due to switching of inductive loads, and it must be physically close
to the OUT and GND pins.
Thermal Considerations: when properly mounted,
the PowerPAD package provides significantly greater cooling ability. To operate
at rated power, the PowerPAD must be soldered directly to the board GND plane
directly under the device. Other planes, such as the bottom side of the circuit
board, can be used to increase heat sinking in higher current applications.