For this design example, use the following input parameters:
- The TPS2001EDBV operates from a 5-V to ±0.5-V
input rail.
- What is the normal operation current, for
example, the maximum allowable current drawn by
portable equipment for BC1.2 is 1500 mA, so the
normal operation current is 1500 mA, and the
minimum current limit of power switch must exceed
1500 mA to avoid false trigger during normal
operation. For the TPS2001E device, target 2-A
continuous output current application.
- What is the maximum allowable current provided by
up-stream power, the maximum current limit of power switch that must lower it to ensure
power switch can protect the up-stream power when overload is encountered at the output
of power switch. For the TPS2001E device, the maximum IOS is 3.5 A.