SLVSFL4 June 2020 TPS2124
PRODUCTION DATA.
In this mode of operation, the device will use an internal comparator between the two inputs to determine the priority source. If both PR1 and SEL are below VREF, priority is given to the highest input voltage. If both of the inputs voltages are equal, VCOMP and hysteresis ensures that IN2 takes priority. If IN2 falls below the VCOMP hysteresis, then IN1 will have priority. If IN2 gets reapplied, it will take priority when it falls within VCOMP of IN1.
In this example, the TPS2124 is configured with two 5-V inputs. When IN2 is applied to the system, it takes priority over IN1. Once it gets removed, priority returns to IN1.