SLVSFL4 June 2020 TPS2124
PRODUCTION DATA.
Table 3 summarizes the applications highlighted in the following sections.
MODE | DEVICE | DESCRIPTION | SECTION |
---|---|---|---|
Manual Switchover | TPS2124 | An external controller (such as an MCU) can be used to manually select between the two input sources. | Manual Switchover Schematic |
Highest Voltage Operation (VCOMP) | TPS2124 | The device automatically selects the highest voltage supply to power the output. | Highest Voltage Operation (VCOMP) |