SLVSFJ2B December 2020 – February 2023 TPS22950
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The current limit is adjusted by connecting an external resistor from the ILIM pin to GND. The current limit resistor can be chosen using the equation:
The units for the equation are amps for ILIM and kilohms for RILIM. For the TPS22950L, the device is only limiting current during a short period of time. Therefore, the peak value of the current (ILIM,PEAK) may be more applicable for system considerations. The equation for this parameter is below: