SLVSDF9A December 2017 – January 2019 TPS23523
PRODUCTION DATA.
In this state the hot swap is fully on and the operation is set as follows:
If any of the following occur, the controller will be kicked back to the OFF state:
Note that if the input voltage is outside the valid range or the fast trip is triggered, the hot swap FET will turn off, but the controller will not exit the Normal Operation state. In this case the PG signal would go low immediately. If this condition persists, the PG_degl will go low as well and the controller would move to the OFF state. This operation prevents the controller from re-starting the system during quick transients.