SLUSBX9I March 2014 – July 2019 TPS23861
PRODUCTION DATA.
RSnA / RSnB: Place according to Figure 60 in a manner that facilitates a clean Kelvin connection with KSENSEA/B.
QPn: Place QPn around the TPS23861 as illustrated in Figure 61. Provide sufficient copper from QPn-D to FPn.
RDRNn: Place RDRNn near to QPn-D. Connect to DRAINn pins as illustrated in Figure 61.
RSENn: Place RSENn near to QPn-S. Connect to SENn pins as illustrated in Figure 61.
FPn, CPn, DPnA, DPnB: Place this circuit group near the RJ45 port connector (or port power interface if a daughter board type of interface is used as illustrated in Figure 61). Connect this circuit group to QPn-D / GND (TPS23861-AGND) using low inductance traces.