4 Revision History
Changes from H Revision (November 2017) to I Revision
- Added figure titles to the Application CurvesGo
Changes from G Revision (October 2016) to H Revision
- Deleted "or unknown" from Auto subsectionGo
- Deleted "and Auto Modes" from TSTART Indicators of Detect and Class Failures subsectionGo
- Changed fault conditions for Auto mode in Detect and Class Failure Indicators tableGo
- Added information to Step 2 in Start/ILIM Event Register subsectionGo
Changes from F Revision (July 2016) to G Revision
- Deleted the MAX value of 150 mA from IGO- in the Electrical CharacteristicsGo
Changes from E Revision (March 2016) to F Revision
- Legacy Device Detection, Changed the paragraph, "in general,..."Go
- Changed section From: Independent Operation when the Bit is Set To: Independent Operation when the AUTO Bit is SetGo
- I2C Slave Address and AUTO Bit Programming, Added NOTE: "When using I2C scan..."Go
- Start/ILIM Event Register, Changed the third list item From: "Detect fault or classification unknown,.." To: "Overcurrent or class mismatch on second finger in Semi-Auto or Manual Mode." Go
- Timing Configuration Register, Added new NOTE under TLIM[1:0]: " If ILIM and ICUT are set to same value..."Go
- Timing Configuration Register, Added new NOTE under TICUT[1:0]: " If ILIM and ICUT are set to same value..."Go
- Two-Event Classification Register, Changed the second list item to include: "CLEn is set or a" Go
- Replaced Figure 58Go
Changes from D Revision (September 2015) to E Revision
- Added note in Features, "Semi-Automatic Mode "Go
- Updated Pin Functions tableGo
- Added new Figure 37Go
- Added new Functional Block DiagramGo
- Changed note in A/D Converter and I2C InterfaceGo
- Changed the Note in I2C Slave Address and AUTO Bit ProgrammingGo
- Added note to I2C Slave Address and AUTO Bit ProgrammingGo
- Changed I2C slave address register note.Go
- Added new Figure 43Go
- Added a note to Manual about type 2 power 2 event classification.Go
- Added content to Semi-AutoGo
- Added "PoEPn" column to Bits DescriptionGo
- Added a note to PoE Plus RegisterGo
Changes from C Revision (June 2015) to D Revision
- Added reference note to Figure 5 and Figure 6Go
- Changed RESET note to add addition reference link. Go
- Added SDAO pin note. Go
- Changed I2C Slave Address and AUTO Bit Programming note. Go
- Added Figure 42, I2C/SMBus Interface Slave Address Programming Protocol. Go
- Added note 3 to Table 10Go
- Changed Connections on Unused Ports section.Go
- Added reference link to the VPWR-RESET Sequencing note.Go
Changes from B Revision (April 2015) to C Revision
- Added Figure 5 and Figure 6Go
- Changed Figure 36, Disconnected AIN pin from GNDGo
- Added SHTDWN note.Go
- Added RESET note. Go
- Added Device Power On Initialization sectionGo
- Added note 2 to Table 10Go
- Added Port n Status Register note.Go
- Added Operating Mode Register Command note. Go
- Added Operating Mode Register Bit Description note. Go
- Added Detect/Class Enable Register Command note. Go
- Added Detect/Class Restart Register Command note.Go
- Added Power Enable Register Command note.Go
- Added Power Enable Register Bit Descriptions note.Go
- Added Reset Register Command note.Go
- Added Reset Register Bit Descriptions note. Go
- Changed Figure 46, Disconnected AIN pin from GNDGo
- Changed Figure 48, Disconnected AIN pin from GNDGo
- Changed Figure 49, Disconnected AIN pin from GNDGo
- Changed Figure 50, Disconnected AIN pin from GNDGo
- Changed QPn description in Per Port ComponentsGo
- Changed maximum VDD supply current from 10 mA to 6 mA in first paragraph and changed wording in second paragraph of VDD.Go
- Added VPWR-RESET SequencingGo
Changes from A Revision (June, 2014) to B Revision
- Changed VDD current consumption from 10 mA (MAX) to 6.0 mA (MAX)Go
- Deleted Processor watchdog trip delay specification.Go
- Added When using the I2C interface note. Go
- Added When using the I2C interface note. Go
- Changed FULL SCALE VALUE from 146.2°C to 150°C (typical).Go
- Changed LSB VALUE from 0.652°C to 7°C.Go
- Added Temperature sensor performance note.Go
Changes from * Revision (March 2014) to A Revision
- Added full TPS23861 IEEE 802.3at Quad Port Power-over-Ethernet PSE Controller datasheet. Go