To start the procedure, the total resistance, including power switch rDS(on) and wire resistance R(WIRE), must to be known.
- Choose R(G) following the voltage-regulator feedback resistor-divider design guideline.
- Calculate R(FA) according to Equation 1.
Equation 1. - Calculate R(FB) according to Equation 2.
Equation 2. - C(COMP) in parallel with R(FA) is needed to stablilize V(OUT) when C(OUT) is large. Start with C(COMP) ≥ 3 × G(CS) × C(OUT), then adjust C(COMP) to optimize the load transient of the voltage regulator output. V(OUT) stability should always be verified in the end application circuit.