CRX: Place CRX1 and CRX2 in line with the CC1 and CC2 traces as shown in Figure 26. These should be placed within one inch from the Type C connector. Minimize stubs and tees from on the trace routes.
Q1: Place Q1 in a manner such that power flows uninterrupted from Q1 drain to the Type C connector VBUS connections. Provide adequate copper plane from Q1 drain and source to the interconnecting circuits.
RS: Place RS as shown in Figure 74 to facilitate uninterrupted power flow to the Type C connector. Orient RS for optimal Kelvin sense connection/routing back to the TPS25741 or TPS25741A. In high current applications where the power dissipation is over 250 mW, provide an adequate copper feed to the pads of RS.
RG: Place RG near Q1 as shown in Figure 74. Minimize stray leakage paths as the GDNG sourcing current could be affected.
RSLEW/CSLEW: Place RSLEW and CSLEW near RG as shown in Figure 74.
RDSCG: Place on top of the VBUS copper route and connect to the DSCG pin with a 15 mil trace.
RF/CF: When required, place RF and CF as shown in Figure 74 to facilitate the Kelvin sense connection back to the device.
CVBUS/DVBUS: Place CVBUS and DVBUS within one inch of the Type C connector and connect them to VBUS and GND using adequate copper shapes.
RSEL/RPCTRL: Place RSEL and RPCTRL near the device.