SLVSGO0 October 2024 TPS25763-Q1
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The NTC pin is used by the device firmware to monitor system temperature. Rising or falling voltages on the NTC pin indicate increasing or decreasing system temperatures, respectively. To achieve a positive temperature slope on the TPS25763-Q1 NTC pin, thermistors can be connected to LDO_3V3 as shown in Figure 8-43.
See Figure 8-44 and Figure 8-45. Using the application configuration GUI, the user can configure system power management responses for up to three VNTC voltages.