SLVSGX1A July 2023 – October 2023 TPS25984
PRODUCTION DATA
The TPS25984x implements undervoltage lockout on VDD and VIN in case the applied voltage becomes too low for the system or device to properly operate. The undervoltage lockout has a default internal threshold of VUVP on VDD and VUVPIN on VIN. Alternatively, the UVLO comparator on the EN/UVLO pin allows the undervoltage protection threshold to be externally adjusted to a user defined value. Figure 8-1 and Equation 1 show how a resistor divider can be used to set the UVLO set point for a given voltage supply.
The EN/UVLO pin implements a bi-level threshold.