SLVSFQ6A November 2020 – June 2021 TPS2640
PRODUCTION DATA
During start-up, as the output capacitor charges, the voltage difference across the internal FET decreases, and the power dissipation decreases. Typical ramp-up of the output voltage, inrush current and instantaneous power dissipated in the device during start-up are shown in Figure 10-2. The average power dissipated in the device during start-up is equal to the area of triangular plot (red curve in Figure 10-3) averaged over tdVdT.
VIN = 24 V | CdVdT = 2.2 μF | COUT = 2.2 mF |
VIN = 24 V | CdVdT = 2.2 μF | COUT = 2.2 mF |
The inrush current is determined as shown in Equation 14.
Average power dissipated during start-up is given by Equation 15.
Equation 15 assumes that the load does not draw any current until the output voltage reaches its final value.