SLVSFQ6A November 2020 – June 2021 TPS2640
PRODUCTION DATA
The TPS26400 incorporate circuitry to protect the system during overvoltage conditions. A voltage more than V(OVPR) on OVP pin turns off the internal FET and protects the downstream load. To program the OVP threshold externally, connect a resistor divider from IN supply to OVP terminal to RTN as shown in Figure 9-1. The TPS26400 also feature a factory set 33-V Input overvoltage cut off V(IN_OVP) threshold with a 2-V hysteresis. This feature can be enabled by connecting the OVP terminal directly to the RTN terminal. Figure 7-26 illustrates the overvoltage cut-off functionality.
Programmable output overvoltage clamp can also be achieved using TPS26400 by connecting the resistor ladder
from Vout to OVP to RTN as shown in Figure 9-2 . This results in clamping of output voltage close to OVP setpoint
by resistors R4 and R5. as shown in Figure 9-3. This scheme will also help in achieving minimal system Iq
during off state. For this OVP configurataion, use R4 > 90 kΩ.