SLVSF24C december 2020 – may 2023 TPS272C45
PRODUCTION DATA
The ground connection can be lost either on the device level or on the module level. If the ground connection is lost, both the channel outputs are disabled irrespective of the EN input level. If the switch was already disabled when the ground connection was lost, the outputs remain disabled even when the channels are enabled. The steady state current from the output to the load that remains connected to the system ground is below the level specified in the Specifications section of this document. When the ground is reconnected, normal operation resumes.