SLVSF24C december 2020 – may 2023 TPS272C45
PRODUCTION DATA
The TPS272C45 includes a temperature sensor on the power FET and also within the controller portion of the device. The device registers a thermal shutdown fault:
After the fault is detected, the switch turns off. If TJ,FET passes TABS, the fault is cleared when the switch temperature decreases by the hysteresis value, THYS. If instead the TREL threshold is exceeded, the fault is cleared after TRETRY passes.
Each channel shuts down independently in case of a thermal event, as each has its own temperature sensor and fault reporting.