SLVSFZ1 December 2020 TPS27SA08-Q1
PRODUCTION DATA
While the switch is disabled, if DIA_EN is high, an internal comparator will detect the condition of VOUT. If the load is disconnected (open load condition) or there is a short to supply theOUT voltage will be higher than the open load threshold (VOL,off) and a fault is indicated on the SNS pin. An internal pull-up of 1 MĪ© is in series with an internal MOSFET switch, so no external component is required if only a completely open load needs to be detected. However, if there is significant leakage or other current draw even when the load is disconnected, a lower value pull-up resistor and switch can be added externally to set the VOUT voltage above the VOL,off during open load conditions.
The detection circuitry is only enabled when DIA_EN = HIGH and EN = LOW.
If VOUT > VOL, the SNS pin will go to the fault level.
If VOUT < VOL, then there is no fault indication.
The fault indication will only occur if the SEL1 pin is set to diagnose the channel.
While the switch is disabled and DIA_EN is high, the fault indication mechanisms will continuously represent the present status. For example, if VOUT decreases from > VOL to < VOL, the fault indication is reset. Additionally, the fault indication is reset upon the falling edge of DIA_EN or the rising edge of EN.