SNVSCF7A December 2022 – August 2024 TPS3435
PRODUCTION DATA
The TPS3435 offers one or two SET pins based on the pinout option selected. SET pins offer flexibility to the user to program the tWD timer on the fly to meet various application requirements. Typical use cases where SET pin can be used are:
The tWD timer value for the device is combination of timer selection based on the CWD pin or fixed timer value along with SET pin logic level. The base tWD timer value is decided based on the Watchdog Time selector in the Section 4 section. The SET pin logic level is decoded during the device power up. The SET pin value can be changed any time during the operation. SETx pin change which leads to change of watchdog timer value or enable disable state, terminates the ongoing watchdog frame immediately. SETx pins can be updated when WDO output is asserted as well. The updated tWD timer value is going be applied after output is deasserted and the tSD timer is over or terminated.
For a pinout which offers only SET0 pin to the user, the tWD multiplier value is decided based on the Watchdog Time Scaling selector in the Section 4 section. Table 7-1 showcases an example of the tWD values for different SET0 logic levels when using Watchdog Time setting as option D = 10ms.
WATCHDOG TIME SCALING SELECTION | tWD | |
---|---|---|
SET0 = 0 | SET0 = 1 | |
A | 10ms | 20ms |
B | 10ms | 40ms |
C | 10ms | 80ms |
D | 10ms | 160ms |
E | 10ms | 320ms |
F | 10ms | 640ms |
G | 10ms | 1280ms |
For pinouts which offer both SET0 & SET1 pins to the user, the tWD multiplier value is decided based on the Watchdog Time Scaling selector in the Section 4 section. Two SETx pins offer 3 different time scaling options. The SET[1:0] = 0b'01 combination disables the watchdog operation. Table 7-2 showcases an example of the tWD values for different SET[1:0] logic levels when using Watchdog Time setting as option G = 100ms. The package pin out selected does not offer WD-EN pin.
WATCHDOG TIME SCALING SELECTION | tWD | |||
---|---|---|---|---|
SET[1:0] = 0b'00 | SET[1:0] = 0b'01 | SET[1:0] = 0b'10 | SET[1:0] = 0b'11 | |
A | 100ms | Watchdog disable | 200ms | 400ms |
B | 100ms | Watchdog disable | 400ms | 800ms |
C | 100ms | Watchdog disable | 800ms | 1600ms |
D | 100ms | Watchdog disable | 1600ms | 3200ms |
E | 100ms | Watchdog disable | 3200ms | 6400ms |
F | 100ms | Watchdog disable | 6400ms | 12800ms |
G | 100ms | Watchdog disable | 12800ms | 25600ms |
Selected pinout option can offer WD-EN pin along with SET[1:0] pins (Pin Configuration C). With this pinout, the WD-EN pin controls watchdog enable and disable operation. The SET[1:0] = 0b'01 combination operates as SET[1:0] = 0b'00.
Make sure the tWD value with SETx multiplier does not exceed 640s. If a selection of timer and multiplier results in tWD > 640s, the timer value is restricted to 640s.
Figure 7-9 to Figure 7-11 diagrams show the timing behavior with respect to SETx status changes.