SNVSBZ2E March 2021 – December 2023 TPS3704
PRODUCTION DATA
Determine which version of the TPS3704x best suits the monitored rail (VMON) and window tolerances found on Table 9-3. The TPS3704x allows overvoltage and undervoltage monitoring for precise voltage supervision of common rails between 0.4 V and 5.55 V. This application calls for very tight monitoring of the rail with only ±5% of variation allowed on the 1.2-VCORE rail. To ensure this requirement is met, the TPS37042 was chosen for its ±3% thresholds. The 3.3-VI/O is more flexible and can operate up to 8% variance. Since the TPS3704x comes in various tolerance options, the ±6% thresholds can be chosen for this voltage rail. To calculate the worst-case for VIT+(OV) and VIT-(UV), the accuracy must also be taken into account. The worst-case for VIT+(OV) and VIT-(UV) can be calculated shown in Equation 5 and Equation 6 respectively:
Hysteresis is also needed to be taken into account when determining the OV and UV thresholds such that the release point after the fault is higher than the power supply tolerance limits. Refer to Figure 6-1 for more details.
When the outputs switch to a high impedance state, the rise time of the RESETx/RESETx pin depends on the pull-up resistance and the capacitance on that node. Choose pull-up resistors that satisfy both the downstream timing requirements and the sink current required to have a VOL low enough for the application; 10 kΩ to 1 MΩ resistors are a good choice for low-capacitive loads.