Make sure that the connection to the VDD pin is low impedance. Good analog design practice is to place a greater than 0.1µF ceramic capacitor as near as possible to the VDD pin.
For noisy envirionments and to improve noise immunity on the SENSE pins, an optional 1nF capacitor between the SENSE pin and GND can reduce the sensitivity to transient voltages on the monitored signal. An alternative to improve noise immunity is to use the CTS feature.
If a capacitor is used on CTS or CTR, place these components as close as possible to the respective pins. If the capacitor adjustable pins are left unconnected, make sure to minimize the amount of parasitic capacitance to not affect the TPD or tCTR.
Place the pull-up resistors on RESET as close to the pin as possible.
When laying out metal traces, separate high voltage traces from low voltage traces as much as possible.
Do not have high voltage metal pads or traces closer than 20mils (0.5mm) to the low voltage metal pads or traces.